AURIX™ Development Studio Forum Discussions
Hello,
I basically wondered what is the C++ Standard Container support in ADS + Tasking like?
I am developing a demo application for a TC397XA where I am trying to use an unordered_map as a buffer.
Both implementing it within a buffer class or instantiating unordered_map in my main code for CPU0 and adding some elements compiles sucessfully but it is met with a trap (Data Access Synchronous Error or Memory Protection Null Address) from the things I have tried while debugging the application with miniWiggler.
Another question I have when it comes to containers is related to vectors. I had to replace the file in the folder "include.cxx" within Tasking compiler sources to be able to compile a project with them by the file in: Vector
But even so, I am not able to verify if the container is working properly since I am not able to see the values it contains when using debugging Expressions suchs as my_vector[0].
If anybody has some guidance or any clues, suggestions are very welcomed! thank you
Show LessI have found what we believe to be a bug regarding OneEye.
When max is set to 1023 and tick-count is set to 100 in the Dial widget with 10-bit bit field signals specified as data-out or auto-connect, the Dial widget freezes when it is moved. It also freezes at max 1010,1018,1019,1021,1022. However, it does not freeze at 1020.
In this case, it did not freeze under the following conditions
- Tick-count=1
- Tick-count = max value
- The max value is divisible by the Tick-count value
The 10-bit bit field signal is obtained from an elf file compiled by TASKING.
Dear developer, would you please investigate and bugfix this issue.
Best Regards,
Show Less1. I got the evaluation version of Infineon MCAL and have installed EBTresos tool. I also installed MC-ISAR_AS422_TC3xx_DEMO_1.40.0.exe and selected the TC37X MCU.
2. I started configurations for MCU module in EBTresos. After configuration I am able to generate "Mcu_PBcfg.c" and other files.
3. After Step#2, how do I integrated this with static MCAL files and create a build ? Should I use the AURIX Development Studio to do this or do I need to use BIFACES interface ?
Where can I get some information about the work flow. Any help on this will be greatly appreciated. Show Less
where can i find the interrupt vector table?
i´m working with TC387 and the Aurix Development Studio.
Thanks in advance and best regards H. Show Less
After commenting the line, the warning in the scr_a2g.h file still appear, when compiling. Please advise how to remove this warning. AURIX-Studio v1.9.0.
#define LABEL_scr_xram__00105 (411) /*(0x19b) */
//#define LABEL_scr_xram__00101 (423) /*(0x1a7) */
Building file: ../scr_a2g.c
ctc W504: ["..\scr_a2g.h" 26/9] macro "LABEL_scr_xram__00101" redefined
Invoking: TASKING C/C++ Compiler
ctc I801: ["..\scr_a2g.h" 23/9] previous definition of macro "LABEL_scr_xram__00101"
0 errors, 1 warnings
Dear Friends,
I am bird in building software. I am using HighTec Development Platform 2.0 (free version). I want to build a few source files and header files into a library file .a
How do I do that?
Thank you for your teaching.
Show LessRegister SMU_FSP displays correct value, but wrong description in the debugger view.
.B.MODE = 2 (Bi-stable protocol) --> shall be Time switching protocol.
ADS Version 1.6.0 debugging on TC397.
Show LessI am trying to build a project in Aurix Dev Studio Version: 1.8.0. I get the below error during linking time.
TASKING VX-toolset for AURIX Development Studio (non-commercial): control program v1.1r8 Build 22011964
Building target: demoproject.elf
ltc E821: ["C:\Infineon\AURIX-Studio-1.8.0\plugins\com.infineon.aurix.tools_1.8.0\build_system\tools\Compilers\Tasking_1.1r8\ctc\include.lsl\tc_mc_arch.lsl" 15/14] syntax error: two architectures defined with name TC
Invoking: TASKING Linker
ltc F018: Invalid LSL file, aborting...
So far I have not been able to figure out what could be the issue. I have also tried to understand how lsl files are designed but nothing seems to be resolving the issue.
Have anyone on this forum faced it and how did you resolve it? Any leads would be much appreciated!
TIA 🙂
Show LessHi there I'm attempting to run ADS on windows in a headless build mode but I'm encountering some errors. I initially used the command
"C:\Infineon\AURIX-Studio-1.8.0\Aurix-studioc.exe" -nosplash -data . -application com.tasking.managedbuilder.headlessbuild -cleanBuild all
this initially caused me some issue as I got complaints about "-perspective" being an invalid argument. I managed to solve this by making a second launcher ini with the "-perspective" argument removed. this made the command:
"C:\Infineon\AURIX-Studio-1.8.0\Aurix-studioc.exe" -nosplash -data . -application com.tasking.managedbuilder.headlessbuild -cleanBuild all --launcher.ini "C:\Infineon\AURIX-Studio-1.8.0\Aurix-studio-headless.ini"
This allows me to build the the projects (just some example project, which build perfectly fine if running in gui) and I get all the expected outputs for both projects in the workspace, with both Debug and Release built. however at the very end i then get an error pop up, informing me that there has been an error and to check the log file. I've attached the log file to this post and I was hoping someone might be able to help me figure out what's breaking
Thanks
Show Less