Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Development Studio Forum Discussions

User22281
AURIX™ Development Studio
Dear Aurix Experts, I am using Aurix Development Studio v1.5.0 to develop an application consisting of a library project and an application project in... Show More
User22281
AURIX™ Development Studio
Dear Aurix experts, I am using Aurix Development Studio v1.5.0 with Tasking tools for a TC36x microcontroller. To increase code reusability, I have mo... Show More
User22074
AURIX™ Development Studio
Hello,I have never worked with multicore microcontrollers and I am trying to figure out how AURIX TC375 is working (it has 3 cores). I am using Multic... Show More
User22447
AURIX™ Development Studio
Hello team, I am using the demo example from https://github.com/Infineon/AURIX_code_examples/tree/master/code_examples here. In MBIST demo example, de... Show More
Louis_LEE
AURIX™ Development Studio
Hi, All and Infineon employee I think Aurix TC237 iLLD code has had error about Qspi communication. I’m using the TFT LCD operating code which is extr... Show More
aditya_barve
AURIX™ Development Studio
Hello,  The kit_a2g_tc332_5v_trb evaluation kit is available with us. To try out some example code I checked the git-hub location for sample code, how... Show More
xukai
AURIX™ Development Studio

AURIX development studio cannot compile xxx .S and xxx.asm assembly files,How to use IDE to compile xxx.s and xxx.asm assembly files

ldj979
AURIX™ Development Studio
Hello aurix users I connect the tc375tp board made with a custom board and the dap mini wiggler and try to debug using the tasking complier in aurix d... Show More
User22023
AURIX™ Development Studio
Hello, is it possible to select which USB-Port should be used to flash the Board? I want to work over an remote PC, where two Boards are connected and... Show More
Orange
AURIX™ Development Studio
I used the Matlab for coding and I use embedded coder to generate c++ code. When I use the Aurix development studio, How I build the generated code on... Show More
Forum Information

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).