Recent discussions
Sort by:
AURIX™ Development Studio
I downloaded the program through the site below.Integrated Development Environment ( IDE ) : AURIX™ Development Studio installationsite : https://www.infineon.com/cms/en/product/promopages/aurix-development-studio/#...
Show More
I downloaded the program through the site below.
Integrated Development Environment ( IDE ) : AURIX™ Development Studio installation
site : https://www.infineon.com/cms/en/product/promopages/aurix-development-studio/#
However, when installing the program, an error as shown below occurs.

I downloaded and tried it several times and ran it on another computer but got the same error.
Is the program on the site a normal program? Show Less
Integrated Development Environment ( IDE ) : AURIX™ Development Studio installation
site : https://www.infineon.com/cms/en/product/promopages/aurix-development-studio/#
However, when installing the program, an error as shown below occurs.
I downloaded and tried it several times and ran it on another computer but got the same error.
Is the program on the site a normal program? Show Less
AURIX™ Development Studio
Hi all,i try the AURIX™ Development Studio and saw that it comes with the tasking c++ compiler (cctc). But in the IDE i can´t compile C++ code. Only t...
Show More
Hi all,
i try the AURIX™ Development Studio and saw that it comes with the tasking c++ compiler (cctc). But in the IDE i can´t compile C++ code. Only the TASKING C Compiler is displayed In Properties->C/C++ Build->Settings->Tool Settings.
Is there a way to compile C++ Files or do i need an other IDE?
Thank you
- Timo Show Less
i try the AURIX™ Development Studio and saw that it comes with the tasking c++ compiler (cctc). But in the IDE i can´t compile C++ code. Only the TASKING C Compiler is displayed In Properties->C/C++ Build->Settings->Tool Settings.
Is there a way to compile C++ Files or do i need an other IDE?
Thank you
- Timo Show Less
AURIX™ Development Studio
HelloI use aurix development studio to learn AURIX tc297.when I used the demo "CCU6_PWM_Generation" to generate the PWMs with a lower frequency, for e...
Show More
Hello
I use aurix development studio to learn AURIX tc297.
when I used the demo "CCU6_PWM_Generation" to generate the PWMs with a lower frequency, for example 5000Hz (modify the marco "#define PWM_FREQUENCY 5000"), I cannot get a valid pwm signal.
I check the code some time, and not find any reason, can any one can help me?
Thank you. Show Less
I use aurix development studio to learn AURIX tc297.
when I used the demo "CCU6_PWM_Generation" to generate the PWMs with a lower frequency, for example 5000Hz (modify the marco "#define PWM_FREQUENCY 5000"), I cannot get a valid pwm signal.
I check the code some time, and not find any reason, can any one can help me?
Thank you. Show Less
AURIX™ Development Studio
Hi,I am trying to develop and execute a sample code for Infineon SAK-TC397XE-256F300S. I was looking into AURIX development studio but it is having on...
Show More
Hi,
I am trying to develop and execute a sample code for Infineon SAK-TC397XE-256F300S.
I was looking into AURIX development studio but it is having only TC2xx series controller supported code reference.
Is there any sample code package example with the startup script and elf file ??
Thank you
Vignesh Show Less
I am trying to develop and execute a sample code for Infineon SAK-TC397XE-256F300S.
I was looking into AURIX development studio but it is having only TC2xx series controller supported code reference.
Is there any sample code package example with the startup script and elf file ??
Thank you
Vignesh Show Less
AURIX™ Development Studio
Hi,I am evaluating the Aurix Development Studio and I have created a small project for TC234. My target is to download the ELF file using the UDE debu...
Show More
Hi,
I am evaluating the Aurix Development Studio and I have created a small project for TC234. My target is to download the ELF file using the UDE debugger (rel. 5.00.02) but I am getting an error when I try to load the file:
Error, Core0::UDESymbolEngine, {"Wrong file"}: "C:\AurixStudioWorkspace\TC234_Evr\Debug\TC234_Evr.elf"
Error, Core0::UDESymbolEngine, Error: Unknown file format
I tried to flash the hex file and the code works as expected (it runs on the hw and the led blinks properly).
Any idea why? Do I need to configure any special setting to generate the correct ELF file format?
Thank you.
BR
S Show Less
I am evaluating the Aurix Development Studio and I have created a small project for TC234. My target is to download the ELF file using the UDE debugger (rel. 5.00.02) but I am getting an error when I try to load the file:
Error, Core0::UDESymbolEngine, {"Wrong file"}: "C:\AurixStudioWorkspace\TC234_Evr\Debug\TC234_Evr.elf"
Error, Core0::UDESymbolEngine, Error: Unknown file format
I tried to flash the hex file and the code works as expected (it runs on the hw and the led blinks properly).
Any idea why? Do I need to configure any special setting to generate the correct ELF file format?
Thank you.
BR
S Show Less
- « Previous
- Next »
Forum Information
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code.
Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family.
It supports Microsoft Windows 10 as a host operating system (OS).
Important links
Downloads
Resources
Related Forums