- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
is it possible to select which USB-Port should be used to flash the Board? I want to work over an remote PC, where two Boards are connected and now i want to flash different projects on the boards. I use the Aurix Development Studio and two TC387 Eval Boards.
Thanks and best regards
- Labels:
-
AURIX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
In my case, I am using it with the following settings:
Target Board : TriBoard TC3X7 TH V2.01 - 2EA
Debugger : Trace32 - 2EA
In my office, two Trace32 are each connected to an evaluation board and each connected to a laptop at the same time.
After remotely accessing the laptop from home, connect to the Windows server for development again.
The window server is set to allow access to the laptop's hardware control device, and you can additionally select the USB port you want to use by using "USB redirect"(this is SW tool).
In this way, you can activate only the USB connected to the laptop, and you can flash or debug only the desired board.