- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello community,
I have problem installing the aurixide 1.7.2. When I start the setup the installation hangs at an certain point. I found out that it is because of the DAS 7.3.7 installation, as the IDE also installs this DAS version as parts of the IDE. Similar behavior for the Aurix-studio 1.6 which also seems to install DAS 7.3.7.
When I try to install DAS 7.3.7 before, it also gets stuck at the step shown in the attached picture . The directory "c:\Programmes\DAS64\" has been created but there is no file in this directory. When I try to cancel the installation twice, the installer disappears, but the Task Manager shows that the installer "DAS_V7_3_7_SETUP.exe) remains as a process. A log file is never created.
When I try to perform the installation via the command line in verbose mode (-v), the following output is generated:
D:\>IFW Version: 3.2.2, built with Qt 5.12.7.
Build date: Oct 28 2020
Installer Framework SHA1: 42d81653
[0] Language: de-DE
[0] Arguments: c:\Users\xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx\DAS_V7_3_7_SETUP.exe, -v
[11] Operations sanity check succeeded.
[11] Resource tree:
[11] :/translations
[12] :/translations/ifw_zh_CN.qm
[12] :/translations/qt_da.qm
[12] :/translations/qt_de.qm
[12] :/translations/qt_en.qm
[12] :/translations/qt_es.qm
[13] :/translations/qt_fr.qm
[13] :/translations/qt_ja.qm
[13] :/translations/qt_it.qm
[13] :/translations/qt_pl.qm
[13] :/translations/qt_ru.qm
[13] :/translations/ifw_de.qm
[13] :/translations/ifw_da.qm
[13] :/translations/ifw_es.qm
[13] :/translations/ifw_en.qm
[14] :/translations/ifw_fr.qm
[14] :/translations/ifw_it.qm
[14] :/translations/ifw_ja.qm
[14] :/translations/ifw_pl.qm
[14] :/translations/ifw_ru.qm
[14] :/translations/qt_zh_CN.qm
[14] :/files-to-patch-macx-emb-arm-qt5
[14] :/files-to-patch-windows
[14] :/files-to-patch-linux-emb-arm-qt5-no-bin-patch
[14] :/files-to-patch-linux-emb-arm-qt5
[14] :/files-to-patch-windows-emb-arm-qt5-no-bin-patch
[14] :/files-to-patch-windows-emb-arm
[14] :/files-to-patch-linux-qt5
[14] :/files-to-patch-windows-qt5
[14] :/files-to-patch-linux-emb-arm
[14] :/files-to-patch-windows-emb-arm-qt5
[14] :/files-to-patch-windows-qt5-no-bin-patch
[14] :/files-to-patch-macx
[14] :/files-to-patch-linux-qt5-no-bin-patch
[14] :/files-to-patch-macx-qt5
[14] :/files-to-patch-macx-emb-arm-qt5-no-bin-patch
[14] :/files-to-patch-macx-qt5-no-bin-patch
[14] :/files-to-patch-linux
[14] :/uninstall.png
[15] :/installer.png
[15] :/installer.ico
[15] :/keepinstalled.png
[15] :/installer.icns
[15] :/install.png
[16] :/keepuninstalled.png
[17] :/qgradient
[17] :/qgradient/webgradients.binaryjson
[17] :/metadata
[18] :/metadata/root
[18] :/metadata/root/license.txt
[19] :/metadata/root/page.ui
[19] :/metadata/root/installscript.qs
[19] :/metadata/config
[20] :/metadata/config/config-internal.ini
[21] :/metadata/installer-config
[21] :/metadata/installer-config/controller_qs.qs
[21] :/metadata/installer-config/Watermark_png.png
[22] :/metadata/installer-config/das.ico
[22] :/metadata/installer-config/config.xml
[23] :/metadata/root.64bit
[23] :/metadata/root.64bit/installscript.qs
[24] :/metadata/root.32bit
[24] :/metadata/root.32bit/installscript.qs
[25] :/metadata/Updates.xml
[25] :/metadata/rccprojectxiRGJl.qrc
[715] INFO:Control Script Installer started
[716] INFO:silent install:
[967] INFO:Administrator PRIVILEGES Detected!
[1117] Loaded control script ":/metadata/installer-config/controller_qs.qs"
[1117] Using control script: ":/metadata/installer-config/controller_qs.qs"
[1125] ================IntroductionPageCallback==============
[2306] Url is: "://metadata/"
[2311] Warning: Component root.64bit specifies "Default" property while being not checkable. The "Default" property will get a "false" value.
[2312] Warning: Component root specifies script value for "Default" property while not being a leaf node. The "Default" property will get a "false" value.
[2313] Warning: Component root specifies script value for "Default" property while being not checkable. The "Default" property will get a "false" value.
[2330] ================LicenseAgreementPageCallback==============
[4435] ================StartMenuDirectoryPageCallback==============
[5161] Installation space required: "42.62 MB" Temporary space required: "0.00 Bytes" Local repository size: "0.00 Bytes"
[5165] Tmp and install directories are on the same volume. Volume mount point: "C:\\" Free space available: "90.01 GB"
[5165] ================ReadyForInstallationPageCallback==============
[5905] backup operation: Mkdir
[5905] - arguments: C:/Program Files/DAS64
[5907] Done
[5909] perform operation: Mkdir
[5911] - arguments: C:/Program Files/DAS64
[5912] Done
[5914] Install size: 2 components
[5917] =============CPU Architecture: x86_64=================
[5939] "Execute" as admin: true
[5939] backup root operation: Execute
[5943] - arguments: cmd, /C, setx, /M, DAS_HOME, C:\Program Files\DAS64, UNDOEXECUTE, cmd, /C, reg, DELETE, HKLM\SYSTEM\CurrentControlSet\Control\Session Manager\Environment, /v, DAS_HOME, /f
[5949] Done
[5950] perform root operation: Execute
[5951] - arguments: cmd, /C, setx, /M, DAS_HOME, C:\Program Files\DAS64, UNDOEXECUTE, cmd, /C, reg, DELETE, HKLM\SYSTEM\CurrentControlSet\Control\Session Manager\Environment, /v, DAS_HOME, /f
[5980] cmd" started, arguments: "/C setx /M DAS_HOME C:\\Program Files\\DAS64
Nothing more happens.
Does anyone have a tip?
Best regards,
Thomas
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi ThomasAtCAM,
Before you install DAS7.3.7, please clean registry in attachement.
Hope to get your update.
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank for the support. But unfortunately nothing changes after deleting the registry keys. DAS as well as the Aurix IDE cannot be installed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Thommas,
Do you have adminitrative right on your PC? I have installed ADS1.7.2 and DAS7.3.7, it works.
Or you could use a clean WIN10 to install again?
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello dw,
yes I have adminitrative right on my PC. The DAS installation will not start without administrative rights. It it possible to install DAS and also the Aurix IDE on my private machine. But I can't use this PC in the company for my evaluation of the Aurix.
BR, Thomas
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
First you can try to install 7.3.x on your computer of the office.
The attached listed some occasions.
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello dw,
installing DAS 7.3.7 is not possible. The installation stops at 1% (see attached picture in my first post). As the Aurix IDE 1.7.2 also installs DAS 7.3.7, the installation of the Aurix IDE is not completed.
I give up.
BR, Thomas
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I think your office computer may has some limitation or restriction for DAS installation.
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I don't think so. I was able to install and use some earlier versions. But they used a different installer.
BR, Thomas