It is not possible to install aurixide 1.7.2 or DAS 7.3.7

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
ThomasAtCAM
Level 1
Level 1
First reply posted First question asked Welcome!

Hello community,

I have problem installing the aurixide 1.7.2. When I start the setup the installation hangs at an certain point. I found out that it is because of the DAS 7.3.7 installation, as the IDE also installs this DAS version as parts of the IDE. Similar behavior for the Aurix-studio 1.6 which also seems to install DAS 7.3.7.

When I try to install DAS 7.3.7 before, it also gets stuck at the step shown in the attached picture . The directory "c:\Programmes\DAS64\" has been created but there is no file in this directory. When I try to cancel the installation twice, the installer disappears, but the Task Manager shows that the installer "DAS_V7_3_7_SETUP.exe) remains as a process. A log file is never created. 

When I try to perform the installation via the command line in verbose mode (-v), the following output is generated:

D:\>IFW Version: 3.2.2, built with Qt 5.12.7.
Build date: Oct 28 2020
Installer Framework SHA1: 42d81653
[0] Language: de-DE
[0] Arguments: c:\Users\xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx\DAS_V7_3_7_SETUP.exe, -v
[11] Operations sanity check succeeded.
[11] Resource tree:
[11] :/translations
[12] :/translations/ifw_zh_CN.qm
[12] :/translations/qt_da.qm
[12] :/translations/qt_de.qm
[12] :/translations/qt_en.qm
[12] :/translations/qt_es.qm
[13] :/translations/qt_fr.qm
[13] :/translations/qt_ja.qm
[13] :/translations/qt_it.qm
[13] :/translations/qt_pl.qm
[13] :/translations/qt_ru.qm
[13] :/translations/ifw_de.qm
[13] :/translations/ifw_da.qm
[13] :/translations/ifw_es.qm
[13] :/translations/ifw_en.qm
[14] :/translations/ifw_fr.qm
[14] :/translations/ifw_it.qm
[14] :/translations/ifw_ja.qm
[14] :/translations/ifw_pl.qm
[14] :/translations/ifw_ru.qm
[14] :/translations/qt_zh_CN.qm
[14] :/files-to-patch-macx-emb-arm-qt5
[14] :/files-to-patch-windows
[14] :/files-to-patch-linux-emb-arm-qt5-no-bin-patch
[14] :/files-to-patch-linux-emb-arm-qt5
[14] :/files-to-patch-windows-emb-arm-qt5-no-bin-patch
[14] :/files-to-patch-windows-emb-arm
[14] :/files-to-patch-linux-qt5
[14] :/files-to-patch-windows-qt5
[14] :/files-to-patch-linux-emb-arm
[14] :/files-to-patch-windows-emb-arm-qt5
[14] :/files-to-patch-windows-qt5-no-bin-patch
[14] :/files-to-patch-macx
[14] :/files-to-patch-linux-qt5-no-bin-patch
[14] :/files-to-patch-macx-qt5
[14] :/files-to-patch-macx-emb-arm-qt5-no-bin-patch
[14] :/files-to-patch-macx-qt5-no-bin-patch
[14] :/files-to-patch-linux
[14] :/uninstall.png
[15] :/installer.png
[15] :/installer.ico
[15] :/keepinstalled.png
[15] :/installer.icns
[15] :/install.png
[16] :/keepuninstalled.png
[17] :/qgradient
[17] :/qgradient/webgradients.binaryjson
[17] :/metadata
[18] :/metadata/root
[18] :/metadata/root/license.txt
[19] :/metadata/root/page.ui
[19] :/metadata/root/installscript.qs
[19] :/metadata/config
[20] :/metadata/config/config-internal.ini
[21] :/metadata/installer-config
[21] :/metadata/installer-config/controller_qs.qs
[21] :/metadata/installer-config/Watermark_png.png
[22] :/metadata/installer-config/das.ico
[22] :/metadata/installer-config/config.xml
[23] :/metadata/root.64bit
[23] :/metadata/root.64bit/installscript.qs
[24] :/metadata/root.32bit
[24] :/metadata/root.32bit/installscript.qs
[25] :/metadata/Updates.xml
[25] :/metadata/rccprojectxiRGJl.qrc
[715] INFO:Control Script Installer started
[716] INFO:silent install:
[967] INFO:Administrator PRIVILEGES Detected!
[1117] Loaded control script ":/metadata/installer-config/controller_qs.qs"
[1117] Using control script: ":/metadata/installer-config/controller_qs.qs"
[1125] ================IntroductionPageCallback==============
[2306] Url is: "://metadata/"
[2311] Warning: Component root.64bit specifies "Default" property while being not checkable. The "Default" property will get a "false" value.
[2312] Warning: Component root specifies script value for "Default" property while not being a leaf node. The "Default" property will get a "false" value.
[2313] Warning: Component root specifies script value for "Default" property while being not checkable. The "Default" property will get a "false" value.
[2330] ================LicenseAgreementPageCallback==============
[4435] ================StartMenuDirectoryPageCallback==============
[5161] Installation space required: "42.62 MB" Temporary space required: "0.00 Bytes" Local repository size: "0.00 Bytes"
[5165] Tmp and install directories are on the same volume. Volume mount point: "C:\\" Free space available: "90.01 GB"
[5165] ================ReadyForInstallationPageCallback==============
[5905] backup operation: Mkdir
[5905] - arguments: C:/Program Files/DAS64
[5907] Done
[5909] perform operation: Mkdir
[5911] - arguments: C:/Program Files/DAS64
[5912] Done
[5914] Install size: 2 components
[5917] =============CPU Architecture: x86_64=================
[5939] "Execute" as admin: true
[5939] backup root operation: Execute
[5943] - arguments: cmd, /C, setx, /M, DAS_HOME, C:\Program Files\DAS64, UNDOEXECUTE, cmd, /C, reg, DELETE, HKLM\SYSTEM\CurrentControlSet\Control\Session Manager\Environment, /v, DAS_HOME, /f
[5949] Done
[5950] perform root operation: Execute
[5951] - arguments: cmd, /C, setx, /M, DAS_HOME, C:\Program Files\DAS64, UNDOEXECUTE, cmd, /C, reg, DELETE, HKLM\SYSTEM\CurrentControlSet\Control\Session Manager\Environment, /v, DAS_HOME, /f
[5980] cmd" started, arguments: "/C setx /M DAS_HOME C:\\Program Files\\DAS64

 

Nothing more happens.

Does anyone have a tip?

Best regards,

Thomas

0 Likes
8 Replies
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

https://community.infineon.com/t5/AURIX/Aurix-developement-debug-error-no-das-device-driver/m-p/3673...

Hi ThomasAtCAM,

Before you install DAS7.3.7, please clean registry in attachement.

Hope to get your update.

dw

0 Likes
ThomasAtCAM
Level 1
Level 1
First reply posted First question asked Welcome!

Thank for the support. But unfortunately nothing changes after deleting the registry keys. DAS as well as the Aurix IDE cannot be installed.

0 Likes
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

Hi Thommas,

Do you have adminitrative right on your PC? I have installed ADS1.7.2 and DAS7.3.7, it works.

Or you could use a clean WIN10 to install again?

dw_0-1662445497641.png

dw_1-1662445627398.png

dw

 

 

 

0 Likes
ThomasAtCAM
Level 1
Level 1
First reply posted First question asked Welcome!

Hello dw,

yes I have  adminitrative right on my PC. The DAS installation will not start without administrative rights. It it possible to install DAS and also the Aurix IDE on my private machine. But I can't use this PC in the company for my evaluation of the Aurix. 

 

BR, Thomas

0 Likes
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

https://www.infineon.com/dgdl/Infineon-DAS_Release_Notes-DevelopmentTools-v07_35-EN.pdf?fileId=8ac78...

First you can try to install 7.3.x on your computer of the office.

The attached listed some occasions.

dw

0 Likes
ThomasAtCAM
Level 1
Level 1
First reply posted First question asked Welcome!

Hello dw,

installing DAS 7.3.7 is not possible. The installation stops at 1% (see attached picture in my first post). As the Aurix IDE 1.7.2 also installs DAS 7.3.7, the installation of the Aurix IDE is not completed. 

I give up.

BR, Thomas

0 Likes
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

I think your office computer may has some limitation or restriction for DAS installation.

dw

0 Likes
ThomasAtCAM
Level 1
Level 1
First reply posted First question asked Welcome!

I don't think so. I was able to install and use some earlier versions. But they used a different installer.

BR, Thomas

0 Likes