- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have an AURIX TFT board TC39x running and I have a DAS driver that appears to allow the USB serial port operate properly. This is on a Windows 10 machine. But I need to move everything to a VirtualBox VM. In there I cannot get the DAS driver working properly. It gives an error when I enable that USB device. In the USB device properties it reports:
This device cannot start. (Code 10)
An invalid parameter was passed to a service or function.
Is the problem that the VM is running Windows 11, or is there a known issue running the DAS in a VM?
Is there a workaround? I don't need to run a debugger using the driver - I just need to instantiate a serial port.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I uninstalled Windows 11 and then started over in VirtualBox with Windows 10 and the DAS device driver worked. So it must be a problem with Windows 11, not with the VM.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I uninstalled Windows 11 and then started over in VirtualBox with Windows 10 and the DAS device driver worked. So it must be a problem with Windows 11, not with the VM.