Aurix Development Studio & Bosch MCS Assembler

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
forvia
Level 2
Level 2
First like given 10 sign-ins 5 replies posted

Hej,

i have a BiFaces projects which was using a Tasking Compiler and Bosch MCS Assembler to compile for the MCS.

I can setup Aurix Development Studio and use external Full Version Tasking compiler, but how can i setup Aurix Development Studio in order to use also the Bosch MCS Assembler in the same project?

BR

Forvia

0 Likes
3 Replies
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

Hi forvia,

Please contact Tasking for commercial version support.

https://www.infineon.com/cms/en/tools/aurix-tools/Compilers/TASKING/

dw

0 Likes
forvia
Level 2
Level 2
First like given 10 sign-ins 5 replies posted

You did not get my point, i have commercial versions for Tasking and Bosch MCS Assembler, my question is how can i add the Bosch MCS Assembler to Aurix Development Studio as it was in Bifaces:

Source files get compiled by Tasking.

Asm files for MCS get compiled by Bosch MCS Assembler

Taskin is linking everthing.

0 Likes
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

Hi forvia,

Could you try latest ADS version please? Below the release note for your reference:

Release Notes - AURIX Ease-of-Use - Version AURIX_IDE_1.7.2

Changes implemented in release V1.7.2

Debugger
* Updated winIDEA debugger.
	The update solves the following issues:
		- PPU debugging not working
		- Renaming a project breaks the usage of winIDEA
	The update introduces the following changes
		- Core synchronization on breakpoint hit (all cores are stopped)
* Added link to iSystem website accessible from the Help menu

MCS (GTM) support
* Added external TASKING MCS Toolchain, which allows to build MCS code.

Device Support
* Added support to TC32x devices 

Build Booster
* Build Booster configuration made available through user interface in project settings
* Build Booster operation is now relative to a specific build configuration rather than the whole project,
	in order to allow build configuration with different source paths in the same project
	
Include paths auto-discovery
* Include paths auto-discovery operation is now relative to a specific build configuration rather than the whole project,
	in order to allow build configuration with different source paths in the same project
	
AURIX Profiler
* Added AURIX Profiler

 


 dw

0 Likes