Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Development Studio Forum Discussions

User22074
Level 1
Level 1
First reply posted First question asked
Hello,

I have never worked with multicore microcontrollers and I am trying to figure out how AURIX TC375 is working (it has 3 cores). I am using Multicore_1 example for KIT_AURIX_TC375_LK (presentation, github) and AURIX Development Studio. Basically, this example is using Core2 to toggle global variable, Core1 to turn off LED if this global var is FALSE and Core0 to turn on LED if global var is TRUE. Example imports and compiles nicely, but I have few questions.


  • Memory usage from .map file looks like this
    5196.attach
    Why all instructions (code) are located in PFLASH? I have expected something to be put into PSPR (psram in .map) for each core. When PSPR will be used then?
  • Still, I suppose, it could be correct to store all instructions in PLFASH, but how controller decides on which core to run which instruction? How can I see that in .map file? Or how can I see which core execute what?

  • Furthermore, I have found document "AURIX™ MULTI-CORE TRICORE™ PROGRAMMING ESSENTIALS", where startup procedure is described as
    5197.attach
    But I could not find nothing like "main.c" "startup" or similar in example project. Is it somehow done automatically or hidden in AURIX Development Studio?

  • Another document (TASKING VX-toolset for TriCore User Guide) mentions that
    AURIX TC3xx derivatives support a Program Flash Memory per core (PFLASH0 .. PFLASHn). Where n is the number of cores minus 1. PFLASH memories are located in 3 MB pages. PFLASH core 0 starts at offset 0. For each next core its PFLASH offset is at the next 3 MB offset.

    So I presumed, that .text.Cpu0_Main.core0_main .. .text.Cpu2_Main.core2_main would be located with this 3 MB offset, but according to .map file they are not:
              Section                              | Space addr | Chip addr
    .text.Cpu0_Main.core0_main | 0x80002218 | 0x00002218
    .text.Cpu1_Main.core1_main | 0x803003ec | 0x000003ec
    .text.Cpu2_Main.core2_main | 0x803005d0 | 0x000005d0


    Offset between .core0_main and .core1_main is something like 3 MB (0x30000), but it is not true for offset between .core1_main and .core2_main. Why is that? Is there any other introductionary literature on this topic (AURIX startup code, multicore operation, PSPR/DSPR/PFLASH/LMU usage examples)?
0 Likes
3 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
1. The TC375 has 6 MB of PFLASH, but each core only has 64K of PSPR. Generally, AURIX applications use PSPR for very specific sections of code that require the highest performance. For example: you might use PSPR for Base Trap Vector table, Base Interrupt Vector table, high frequency interrupt functions, Operating System task switch code, etc. Many applications don't use PSPR at all.

2. By default, any core can access any instruction. For most applications, common libraries such as the operating system, MCAL, or iLLD are shared by all cores. There is no way to see what core executes what in the map file. The compiler generally doesn't know what core is executing each function.

3. The startup flow of an ADS project is:
- Configurations/Ifx_Cfg_SswBmhd.c: start address = 0xA0000000
- Lcf_Tasking_Tricore_Tc.lsl
LCF_STARTPTR_NC_CPU0 = 0xA0000000
"__START0" := LCF_STARTPTR_NC_CPU0;
start_address = _START
- Infra/Ssw/TC375/Tricore/Ifx_Ssw_Tc0.c, _START()
- Ifx_Ssw_Tc0.c, __StartUpSoftware() ... __StartUpSoftware_Phase5()
- Ifx_Ssw_Tc0.c, __StartUpSoftware_Phase6(): starts CPUs 1..5
- Ifx_Ssw_Tc0.c, __Core0_start()
- Cpu0_Main.c, core0_main

4. That TASKING document is a little misleading. "Program Flash Memory per core" refers to the fact that each PFLASH physical bank has a local CPU path that is faster than going over the SRI bus. But by default, any CPU core can access any instruction in any PFLASH bank. The default linker setup just allocates functions into all of PFLASH.

Hello,

this made things clearer,

 i still have a question, in ARM based architectures, when i used to do a jump from bootloader to application.

we used to jump to reset handlers which is located in 2n location of the applicatio.hex...

in aurix based, where should i jump to ,to start running my application?

0 Likes
User22074
Level 1
Level 1
First reply posted First question asked
Thank You very much! It is now more clear for me.
0 Likes