Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
harelTur
Level 3
Level 3
25 sign-ins 10 replies posted 10 questions asked

Hi

My board - Murata Type1LD

I try to run test with command : pkteng_start 00:11:22:33:44:55 tx 20 1024 0

The last 0 mean that this test not stop.

In my setup I see the Current and when this command run the current increase to be 11 mA, but after a short time the current return to 3 or 4 mA.

I see the measurment current in my lab power supply/

I use Murata document -added.

1 Solution
MuraliR_36
Moderator
Moderator
Moderator
250 sign-ins 250 replies posted 100 solutions authored

What is the command sequence that you are using here before running pkteng_start command? Is this running with the mfgtest or the production version of the firmware?

View solution in original post

0 Likes
1 Reply
MuraliR_36
Moderator
Moderator
Moderator
250 sign-ins 250 replies posted 100 solutions authored

What is the command sequence that you are using here before running pkteng_start command? Is this running with the mfgtest or the production version of the firmware?

0 Likes