Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SURYASUNDAR
Level 2
Level 2
First like given 50 sign-ins First solution authored
Hi,
   Iam sharing this mail to get the information regarding KitProg3 debugger part in the  CY8CPROTO-062-4343W PSoC 6 WIFI BT prototyping kit. We are facing some issues to isolate the debugger from the kit,How can we  isolate this debugger part to program another hardware CYBLE343072 Module.
 
0 Likes
1 Solution
Ekta_N
Moderator
Moderator
Moderator
750 replies posted First like given 250 solutions authored

Hi @SURYASUNDAR 

Yes, the onboard KitProg3 in the CY8CPROTO-062-4343W kit can be used to program the CYBLE343072 Module using the J6 header. These headers bring out the USB-UART and USB-I2C interfaces pins of the KitProg3.. The CYBLE343072 Module uses kitprog3 as USB-UART bridge for the purpose of programming.
 This is possible only after breaking away the KitProg3 section. Connecting two or more target devices will cause programming to fail.

Ekta_0-1658814411974.png

You can also refer to the CYBLE-343072-EVAL kit which uses kitprog3 as USB-UART bridge for the purpose of programming the module

Best Regards
Ekta




View solution in original post

0 Likes
1 Reply
Ekta_N
Moderator
Moderator
Moderator
750 replies posted First like given 250 solutions authored

Hi @SURYASUNDAR 

Yes, the onboard KitProg3 in the CY8CPROTO-062-4343W kit can be used to program the CYBLE343072 Module using the J6 header. These headers bring out the USB-UART and USB-I2C interfaces pins of the KitProg3.. The CYBLE343072 Module uses kitprog3 as USB-UART bridge for the purpose of programming.
 This is possible only after breaking away the KitProg3 section. Connecting two or more target devices will cause programming to fail.

Ekta_0-1658814411974.png

You can also refer to the CYBLE-343072-EVAL kit which uses kitprog3 as USB-UART bridge for the purpose of programming the module

Best Regards
Ekta




0 Likes