Hi Infineon support team.
I would like to evaluate CYW4373(SDIO) on i.MX8MQ EVK "Android" based on the following URL.
https://www.cypress.com/products/linux-and-android-airoc-wi-fi-bluetooth
In the case of CYW4373(SDIO) connects to the i.MX8MQ uSD slot, please tell me the fdt file for reference.
Thanks,
Tayo
Solved! Go to Solution.
The Android driver package is available at this link https://community.infineon.com/t5/Resource-Library/Infineon-Android-Release-2021-06-29/ta-p/281512 By FDT file, did you mean device tree DTB? During the patching process, the file android_cy_ahd-2021_0629_REL_PKG\cypress\device\imx8mq\android10\aosp-patches\vendor\nxp-opensource\kernel_imx\0001-Add-Cypress-wifi-chip-support-in-Android-10.0.0-2.0..patch is used. In this file, the /arch/arm64/boot/dts/freescale/imx8mq-evk.dts is patched to include the Wi-Fi specific additions.
The Android driver package is available at this link https://community.infineon.com/t5/Resource-Library/Infineon-Android-Release-2021-06-29/ta-p/281512 By FDT file, did you mean device tree DTB? During the patching process, the file android_cy_ahd-2021_0629_REL_PKG\cypress\device\imx8mq\android10\aosp-patches\vendor\nxp-opensource\kernel_imx\0001-Add-Cypress-wifi-chip-support-in-Android-10.0.0-2.0..patch is used. In this file, the /arch/arm64/boot/dts/freescale/imx8mq-evk.dts is patched to include the Wi-Fi specific additions.