AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions
When i jsut connect cyw43439.
I'm check for pinout using osiloscope
Sleep Clock, VDDIO, WL_REG_ON, BT_REG_ON all is okay.
stm32 chip on cts(connecting to cyw43439(rts pin)) it LOW
but stm32 chip on rts(conneting to cyw43439(cts pin)) it is high.
How to solved problem?
Show Less
const uint8_t reset_buff[] = {0x01, 0x03, 0x0C, 0x00};
const uint8_t minidriver_buff[] = {0x01, 0x2E, 0xFC, 0x00};
HAL_UART_Transmit_IT(&huart2, (uint8_t *)reset_buff, sizeof(reset_buff));
HAL_Delay(100);
HAL_UART_Transmit_IT(&huart2, (uint8_t *)minidriver_buff, sizeof(minidriver_buff));
I'm tired reset, download_minidriver.
When i check osilioscope, maybe it was worked.
So Can i firmware intall w_bt_firmware_controller.c for opcode?
Hi Sir,
please provide CYW43439 pcb stack info.
thanks.
Best Regards,
Howard
If i create cy_rtos_create_thread. My all rtos thread broken.
Hello. I am wondering if the CYW55573 can be used with the stm32 according https://github.com/Infineon/AIROC-Wi-Fi-Bluetooth-STM32. And if yes, which stm32 series would be best and which development board? Also, should the CYW55573 be used in a module such as the Sona IF573
Show LessI'm tried porting exmaple(ble_hello_sensor, mfg_test).
but, all project some problem. When i using, maybe cy_rtos is block or dead thread.
So, I can't passing bt_firmware_downlaod()
Can you Check my Codes?
Show Less
When i run ble_hello_sensor, I'm falled HardFault_Handler.
I think cy_rtos_create_thread(cybt_platform_task.c) for TX task, RX task.
I think stop point.
This time not called hardfault_handler but can't init bt_start_fw_download.
help me...
Show LessHi guys,
Would you please inform how to set the multiple SSIDs by calling the function named "whd_wifi_scan" in the WHD ?
Current source code describes as only one SSID set in "CY_WCM_SCAN_FILTER_TYPE_SSID" but I'd like to set the multiple SSIDs for AP scan.
I've used the AIROC-Wi-Fi-Bluetooth-STM32 Expansion Pack 1.5.0(or 1.5.1) with Enterprise-security V2.1.0 from GitHub
on STM32H747DISCO board with Murata 2AE(CYW4373) as a STA.
Regards,
- Chuta_the_Cat
Show Less