AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions
Hi Sir,
please provide CYW43439 pcb stack info.
thanks.
Best Regards,
Howard
If i create cy_rtos_create_thread. My all rtos thread broken.
Hello. I am wondering if the CYW55573 can be used with the stm32 according https://github.com/Infineon/AIROC-Wi-Fi-Bluetooth-STM32. And if yes, which stm32 series would be best and which development board? Also, should the CYW55573 be used in a module such as the Sona IF573
Show LessWhen i run ble_hello_sensor, I'm falled HardFault_Handler.
I think cy_rtos_create_thread(cybt_platform_task.c) for TX task, RX task.
I think stop point.
This time not called hardfault_handler but can't init bt_start_fw_download.
help me...
Show LessHi guys,
Would you please inform how to set the multiple SSIDs by calling the function named "whd_wifi_scan" in the WHD ?
Current source code describes as only one SSID set in "CY_WCM_SCAN_FILTER_TYPE_SSID" but I'd like to set the multiple SSIDs for AP scan.
I've used the AIROC-Wi-Fi-Bluetooth-STM32 Expansion Pack 1.5.0(or 1.5.1) with Enterprise-security V2.1.0 from GitHub
on STM32H747DISCO board with Murata 2AE(CYW4373) as a STA.
Regards,
- Chuta_the_Cat
Show LessI have a stm32H745ZI6 chip and cyw43439(Laird-Sterling-LWB-PLUS) so i doing porting ble_hello_sensor to my chips.
My project is sucess for build, but my chips not showing to my Phone for my BLE(Hello)
STM32CubeIDE version 1.14.1
STM32CubeMX version 6.10.10-RC9
GPIO USART2 RX/TX(CTS/RTS), CYBSP_POWER
TIMER LPTIM1
Can i Connecting BLE to USART? Example connecting to UART.
Show Less测试环境: RK3566 android11 linux4.19内核
测试固件以及驱动patch包,以及抓的dmesg打印和logcat 见附件
目前加载驱动后已经有wlan起来了,但是扫不到设备
The customer is considering either the CYW4373 or CYW54591, but since the end customer uses Android, they want to implement Fluoride. Are these parts compatible with Fluoride?
Show LessHi guys,
Would you please inform if the WPA3 enterprise security 192bit mode can work by using the "Enterprise-security" software ?
The link is
https://github.com/Infineon/enterprise-security
I've developing the WPA3 several client mode using the Infineon's Enterprise-Security and the Airoc-wifi-Bluetooth-STM32.
The EAP-TLS and the EAP-PEAP have been worked correctly but the 192bit mode can not worked.
Thanks,
- Chuta_the_Cat
Show Less