AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions
text.format{('custom.tabs.no.results')}
When i porting wifi_join_wpa3, but I'm get a "Failed to initializze Wi-Fi".
So i'm check problem point. then, i find stop point.
whd_management.c in, whd_management_wifi_platform_init
I'm tried porting exmaple(ble_hello_sensor, mfg_test).
but, all project some problem. When i using, maybe cy_rtos is block or dead thread.
So, I can't passing bt_firmware_downlaod()
Can you Check my Codes?
Show Less
Greetings,
I am trying to integrate LBEE5PK2AE-564 WiFi/BT module with USB interface (using CYW4373E chipset) with imx8mm (Android) and want to test WiFi/BT in Android,
i have tested the WiFi successfully and now trying to integrate and test Bluetooth, but in order to test the Bluetooth we used a binary (brcm_patchram_plus_usb_64bit) to load the firmware in the Linux but in Android the binary does not work as it is different linker.
For Example:
This is the binary you have provided:
# file brcm_patchram_plus_usb_64bit
brcm_patchram_plus_usb_64bit: ELF shared object, 64-bit LSB arm64, dynamic (/lib/ld-linux-aarch64.so.1), BuildID=403983701e4aaf5728177f1e9b6e91db9354cdd1, not stripped
And this is present in our source for reference architecture:
# file cmd
cmd: ELF shared object, 64-bit LSB arm64, dynamic (/system/bin/linker64), for Android 30, BuildID=f97435a45132606a0c701ed5c1709bd5, stripped
And as you can see the dynamic lib linker is different. And when i execute the binary you have provided(given all permissions), I am getting the following error:
phyboard_polis:/vendor/bin # ./brcm_patchram_plus_usb_64bit
/system/bin/sh: ./brcm_patchram_plus_usb_64bit: No such file or directory
1|phyboard_polis:/vendor/bin #
1|phyboard_polis:/vendor/bin # ls -l brcm_patchram_plus_usb_64bit
-rwxr-xr-x 1 root shell 23840 2024-03-18 06:18 brcm_patchram_plus_usb_64bit
So I tried cross compiling by downloading the source code from GitHub but it throwing error. Please have a look at the error:
$ aarch64-linux-gnu-gcc -o brcm_patchram_plus_usb brcm_patchram_plus_usb.c -lbluetooth
brcm_patchram_plus_usb.c: In function ‘hci_send_cmd_func’:
brcm_patchram_plus_usb.c:311:9: warning: implicit declaration of function ‘writev’; did you mean ‘write’? [-Wimplicit-function-declaration]
while (writev(sock, iv, ivn) < 0) {
^~~~~~
write
/usr/lib/gcc-cross/aarch64-linux-gnu/7/../../../../aarch64-linux-gnu/bin/ld: cannot find -lbluetooth
collect2: error: ld returned 1 exit status
And there is no libbluetooth.so in our toolchain.
I request you to provide us with brcm_patchram_plus_usb_64bit binary which supports Android or please provide us with documentation or procedure to compile for Android or is there any another way to run the binary and flash the firmware.
Thanks.
Show LessHi there,
may I ask
1. Does IFX WiFi 2.4G support 18.5dbm power solution?
2. Does IFX BT support apple find my and does it support Android?
Thank you!
Mason
Show LessWhen i porting stm32h745 + Laird(lwb+), but stoped install firmware.
I think bluetooth sensor can't init hello_sensor_application_init();
But nucleo-745zi-q + Lwb(4343w) it's worked.
Show Less
Hi Sir,
Please provide CYW43012 device marking.
Thanks for supports.
Best Regards,
Howard
Hello,
We are using CYW43455 and its godzilla release on linux 5.15.71. Occasionally, when device comes back from deep sleep, CYW43455 shows its connected ( RSSI is being changed when getting closer or further to AP), IP address is there, but the network data doesn't come through. In addition it looks like that Rx counter showed in output of ifconfig command doesn't change when CYW43455 is in this state.
Can you please help solving this issue ? Is this a known issue, is there a patch for it ? Or we would need to come up with mechanism to detect this state and then try some recovery steps (reconnect, interface down/up, reassociate)?
Thanks,
Bogdan
Show LessWe're considering a CYW54590-based wifi/BT module for use in an audio device, and it would be very useful to be able to perform (reasonably) accurate time synchronization between multiple devices. Does the CYW54590 firmware support any mechanism to do so? Support for IEEE 802.1AS (gPTP) clause 12 would be ideal but any other mechanism would be welcome too, even something as basic as the ability to cross-timestamp the TSF timer of the CYW54590 (which is already synced between all devices connected to the same wifi AP) by providing the TSF timestamp of a GPIO pulse.
Show LessHello. I am wondering, to use the CYW55572 in the https://github.com/Infineon/AIROC-Wi-Fi-Bluetooth-STM32, which module should it be integrated in? Is the AW-XH327 module in https://www.azurewave.com/wireless-modules-infineon.html a good solution?
Show Less