AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions
I found the WiFi/Bluetooth module CYW43012C0WKWBGT, which uses the CYW43012 chip. This module fits our design well and we'd like to incorporate it into our schematics, however all I can find online for this module is the data sheet. Is there a footprint and/or schematic symbol available for this product?
Show LessHi sir,
Because using CYW43455 for BQB certification, need to provide "Host QDID". My system is Embedded Linux and uses BlueZ 5.0 Stack. Can the following be used?
QDID 172247
https://launchstudio.bluetooth.com/ListingDetails/134246
Show Less
Hi
Where can I download the report?
Thanks,
I have a CYW954907AEVAL1F evaluation board and I would like to start a wpa3 access point, but the board responds with an 'invalid encryption type' error. Looking at the command list, it appears I can join an access point with wpa3, but I cannot start an access point with wpa3. I'm using the start_ap command, is there another way to do this? Or is that functionality not supported by this eval board? If not, is there an eval board that does support starting wpa3 access points?
Thank you
Show LessPlease provide some ideas why a build of one project fails while others succeed?
Building test.console (a project included with WICED) works fine on two different PCs. Building test.at_cmd (a project provided by Murata) fails on one specific computer. It works on the other computer. The computer it works on has been running WICED for many years. The computer it fails on is at a different company and recently loaded WICED. WICED has been removed and reinstalled several times with no major improvements.
The error is:
libraries/filesystems/ota2/./wiced_ota2_image.c: In function 'wiced_ota2_image_copy_uncompressed_component':
libraries/filesystems/ota2/./wiced_ota2_image.c:577:19: error: 'OTA2_IMAGE_FLASH_BASE' undeclared (first use in this function); did you mean 'PLATFORM_FLASH_BASE'?
The full console output is attached for the PC that fails and for the PC that passes.
Greg
Show Less
Hi,
I am using the CYW43455 core.
The test router provides both 2Ghz and 5Ghz networks with the same ssid.
The scan returns correctly both networks.
I tryied wl join <ssid> -b <bssid> without success
What is actually the right sequence to select one or the other network then to set up the interface ?
Thanks for the help.
Jean-Yves
Show LessI using RaspberryPI4b for test other BLE device.
Maybe because of output from RaspberryPI is weak, it often happens that the device cannot identify RasPI and the test does not proceed.
After investigating, I found out that CYW43455 is used for Raspberry PI.
From the searched information, I tried using hcitool to enter commands (including vendor specific commands), but it did not change or there was an error.
Is there a way to change the TX power?
If you have any documents that describe them, please tell me how to get them.
I am looking to integrate a Wifi6+BLE module solution into our embedded medical device. I wish to browse your datasheet for the Cypress/Infineon CYW55572 module, plus any additional information on integrating it to an ARM Cortex-style MCU. I'd also be interested in learning on other options and solutions from Cypress/Infineon for a handheld medical device.
Show LessDear all,
What command can I set the CYW4373 in PSM and the PSM's setting can I change?(like Beacon interval)
Where the CYW4373's user sheet can I got some advices?
Best Regards,
Hong
Show Less