AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions
Hi,
We created Template Manufacturing Application [Tester - Bluetooth MFG Tool] for CY8CPROTO-062-4343W (PSoC™ 6 Wi-Fi BT Prototyping Kit) via ModusToolBox 3.0 with 'Projector Creator 2.0'.
After Project created / build / download to target board, the 'wmbt' tool is not working.
To make 'Bluetooth MFG Tool' worked, the 'mtb-hal-cat1' library had to downgrade to 'release-v2.1.0'.
What's the major API difference between 'release-v2.1.0' and 'release-v2.3.0' in this application?
Can this template application work with latest CAT1 HAL release?
Also, this Bluetooth MFG tool validated compatibility with MTB 2.2, will this application have MTB v3 support?
Show Less
How is the BLE 2M PHY TX/RX HCI command for CYW89459?
Hello All,
We are using CYW43439 wifi and bluetooth module chip with AM335x. We have downloaded the CYW43439 driver from below link.
As per the documentation available in the driver zip, the backports of this driver are supported Linux kernel above kernel version 3.10. We are trying to compile the driver backports along with Kernel 3.12 by following the steps provided in the documentation, but we are getting below compilation errors.
#
# configuration written to .config
#
Building backport-include/backport/autoconf.h ... done.
CC [M] /home/prathamesh/psk/v5.15.58-backports/compat/main.o
In file included from include/linux/module.h:9:0,
from /home/prathamesh/psk/v5.15.58-backports/backport-include/linux/module.h:3,
from /home/prathamesh/psk/v5.15.58-backports/compat/main.c:1:
/home/prathamesh/psk/v5.15.58-backports/include/linux/list.h: In function 'list_del_init_careful':
/home/prathamesh/psk/v5.15.58-backports/include/linux/list.h:308:2: error: implicit declaration of function 'smp_store_release' [-Werror=implicit-function-declaration]
/home/prathamesh/psk/v5.15.58-backports/include/linux/list.h: In function 'list_empty_careful':
/home/prathamesh/psk/v5.15.58-backports/include/linux/list.h:326:9: error: implicit declaration of function 'smp_load_acquire' [-Werror=implicit-function-declaration]
/home/prathamesh/psk/v5.15.58-backports/include/linux/list.h:326:27: warning: initialization makes pointer from integer without a cast [enabled by default]
In file included from include/linux/stat.h:18:0,
from include/linux/module.h:10,
from /home/prathamesh/psk/v5.15.58-backports/backport-include/linux/module.h:3,
from /home/prathamesh/psk/v5.15.58-backports/compat/main.c:1:
/home/prathamesh/psk/v5.15.58-backports/backport-include/linux/time.h: At top level:
/home/prathamesh/psk/v5.15.58-backports/backport-include/linux/time.h:5:26: fatal error: linux/time64.h: No such file or directory
cc1: some warnings being treated as errors
compilation terminated.
make[5]: *** [/home/prathamesh/psk/v5.15.58-backports/compat/main.o] Error 1
make[4]: *** [/home/prathamesh/psk/v5.15.58-backports/compat] Error 2
make[3]: *** [_module_/home/prathamesh/psk/v5.15.58-backports] Error 2
make[2]: *** [modules] Error 2
make[1]: *** [modules] Error 2
make: *** [modules] Error 2
Could you please help me finding what did go wrong?
Show LessHi,
I was testing BT RF performance of CYW43012 in CY8CKIT-062S2-43012 using CYBluetool. How can I perform Conducted RF tests(like 100% Tx BDR). What physical modification should I make.
Earlier "C49 to C50 and solder a IPX connector on J1, and then connected RF cable" modification was made. But then when I'm executing Set_Tx_Freq_ARM using CYBluetool, I'm getting power as -12dBm, whereas the data sheet value is 13dBm.
What is the correct method to do conducted BLUETOOTH RF test in CYW43012 in CY8CKIT-062S2-43012.
What on and off board modifications should I make?
Regards,
Arun Varghese
Show LessDear Sir,
I Find the web link as below but i don't it know it support wpa2-enterprise and wpa3-enterprise on STM .
chip use
- CYW4373 / CYW4373/E
B.R.
Bill.
Show LessI am using btstack 3.7.1 and would like to use the BLE HID functionality in my project. Which are the components to be included in the makefile to achieve the same.
Show LessPlease tell me where to find the file "FileX_exFAT.TraceX.ARM_CM3.release.a"
Error when building with exFAT library
libraries/filesystems/FileX/exFAT/exFAT.mk:65: libraries/filesystems/FileX/exFAT//../FileX_src.mk: No such file or directory
make.exe[1]: *** No rule to make target 'libraries/filesystems/FileX/exFAT//../FileX_src.mk'. stop.
make: *** No rule to make target 'build/snip.sd_filesystem-CYW954907AEVAL1F/config.mk', needed by 'main_app'. stop.
Hi Sir,
In the CYW43439 Datasheet table 28, show the BT RX sensitivity is -94dBm , GFSK , 0.1%BER, 1Mbps.
but it is not specified BT and BLE such as CYW43012 datasheet.
Could you help to provide CYW43439 BLE sensitivity (1Mbps) for reference.
Show Less
Hardware Setup: CY8C6247FDI-D32 + Murata 1DX based on CYW4343W.
Problem: I'm seeing cyhal_sdio_bulk_transfer failed errors when sending data over wifi. This is the error
Appreciate any thoughts and comments. Please see attached screenshots.
This is the callstack:
cy_rtos_get_semaphore
SDIO_SendCommandAndWait
cyhal_sdio_bulk_transfer
Hi Sir,
Where can I find AIROC Wi-Fi solution's throughput test information, such as test conducted with iPerf in a shielding room?
customer want to know the CYW43012 and CYW4373 throughput in IP layer.
BR,
Jack
Show Less