AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions
Hi Team,
Currently, we would like to implement the PMKID cache functionality for WPA enterprise.
We found the following source code that uses the "IOVAR_STR_PMKID_INFO" command.
We use this to check the PMKID cache, so when we call the command it returns with success.
But, we cannot see the PMKID list in the AssociationRequest when reconnecting to the AP.
We use Murata Wi-Fi module Type2AE (CYW4373E) with reference to the following source code.
Infineon AIROC-Wi-Fi-Bluetooth-STM32 Expansion Pack 1.5.1
Best Regards,
Tsutsumi
Show Less
I'm exploring the possibility of connecting a CYW4373-equipped Type 2BC to the USB HOST port of an STM32MP135 due to the SDIO being occupied by other tasks. I've referred to the document for guidance. Unfortunately, it appears that the Murata uSD-M.2-Adapter doesn’t support USB HOST functionality, necessitating an alternate approach.
Could anyone kindly provide advice on installing relevant drivers, SDK, and necessary software tools? Your insights and guidance on this issue would be greatly appreciated.
Show LessI am working on a project using an Arduino Portenta H7 which comes with a Murata 1DX and I am trying to communicate with it in order to develop a WIFI scan program. I have checked everywhere and I can not seem to find a driver C library (.c and .h files that include function defintions allowing the communication with the Murata 1DX). Does anyone know where I can find a software library for this purpose ?
Thank you
Show LessHello,
I recognize that the auto-reconnection ability is provided by "Wi-Fi Connection Manager Library" and "Enterprise Security Library"(as below).
Here, does the limits about auto-reconnection exists?
For example for the number of reconnection, timeout etc...
Thanks
Show LessCould you provide me the datasheet of CYW89570BFFBGT, please?
版本ifxadh_100.10.80,wl 版本1.363 RC125.7,不支持 ./wl tko 相关命令不支持,具体日志见附件,帮忙看看什么原因,谢谢
# ./wl ver
1.363 RC125.7
wl0: Aug 29 2023 06:27:17 version 13.50.2 (0453ef4 CY) FWID 01-b11790d
#
#
#
# ./wl tko enable '0'
set: error parsing value "enable" as an integer for set of "tko"
var unrecognized name, type -h for help
Show Less
The current new AIROC firmware, which is in the Airoc extension pack 1.5.1 (https://github.com/Infineon/AIROC-Wi-Fi-Bluetooth-STM32) reduces the strength of the RSSI levels.
- Why is that happening?
- Is there a way to have the same RSSI performance as with the 1.5.0 version?
RSSI with Infineon extension pack 1.5.0:
RSSI with Infineon extension pack 1.5.1:
Switch from 1.5.0 to 1.5.1:
Thanks in advance
Show Less