Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions

guliqiang
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
工程师你好!我的问题是这样的,我用你们的开发板CY943907AEVAL1F 可以下载程序,这个开发板上用了USB转JTAG芯片FT2232HQ-TRAY,我们的产品不需要这个芯片,我们想直接用JTAG下载工具连接到LBWA1UZ1GC上下载。现在在这个步骤遇到了困难,不知道开发软件需要怎么设置?请... Show More
mits_4588016
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
I would like to know API for 802.11k and 802.11r for STM32 Expansion pack with CYW4373 like a wwd_wifi_radio_resource_management_beacon_req on wwd_wif... Show More
hawkp
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
I have fast data >200Mbps to be sent out to a Wifi access point. The protocol of this fast data is SLVS.  So I would use an FPGA to convert from SLVS ... Show More
yolominwoo
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
During the project, I need to create equipment that can be updated wirelessly using WiFi. So far, the MCU has been implemented to connect to the route... Show More
Bill_123
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
Hi IFX, 1.May I know CYW43455 support "auto band steering" function? I thinks the function is AP implementation,is right?2.Does CYW43455 support wpa3+... Show More
tstutter
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
My setup: - ARM host processor running 5.15.67 Linux.  - Murata 1MW BT/Wi-Fi combo chip (BCM43455) over SDIO using OOB wakeup - Wi-Fi firmware: versio... Show More
yolominwoo
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
When i reboot mcu with cyw43439(Laird sterling lwb-plus), my ble chips not working. but my mcu system reset 5~10 times it work okay.   Show More
Translation_Bot
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
I'd like to pair with Just Works, is this Bluetooth just turned on by default inside, and then Just Works is used when pairing the phone to the board?... Show More
RohiChand2024
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
Can you please guide if CYW4343W support Hands free profile so that we can use it in smartwatch to transfer phone call from mobile phone to smartwatch... Show More
mits_4588016
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
I use wl 4373.exe with CYW 4373. Are commands such as rrm, rrm_nbr_req, etc. supported by CYW? Because there is no response when I send the following ... Show More