Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SeunghanLim
Level 5
Level 5
Distributor - Changnam (South Korea)
250 sign-ins 50 replies posted 50 questions asked

Hi~ 

 

I tried to promote with CYW43012

They(Customer) want to install CHIP for their own products.

Questions are like as below

 Q1 : They want to CYW43012 as RTOS environments not based on OS(Linux)?

          Is it possible to develop ?

Q2: If CYW43012 can be operated as standalone mode, It will be fit for their requirements.

         Is it possible to be operated as stand alone mode?

Q3: If they want, they can chooose pick one method like as (WIFI only mode, BT Onlymode , WIFI & BT mode)?

Q4: If CYW43012 supports a stand-alone mode, It seems to communicate with SDIO interface and UART.

       If then, They worried about the data transferring speed.

      How fast can they transfer data?

 

Many Thanks

BRs

Daniel Lim

         

Daniel Lim
0 Likes
1 Solution
Phanindra_I
Moderator
Moderator
Moderator
250 sign-ins 10 likes given 25 likes received

Hi,

Q1. They want to CYW43012 as RTOS environments not based on OS(Linux)?

>> Yes, RTOS is supported with CYW43012. You can develop applications based on RTOS for CYW43012.

Q2. Is it possible to be operated as stand alone mode?

>>  Please clarify what you mean. If you are asking about operating CYW43012 without host mcu then answer is no. The wifi applications will run on host mcu, so it cannot be operated stand alone.

Q3. If they want, they can chooose pick one method like as (WIFI only mode, BT Onlymode , WIFI & BT mode)?

>> Yes, it is possible to operate in all the mentioned modes using "WL_REG_ON", "BT_REG_ON" pins.

Q4. How fast can they transfer data?

>> Again, not sure what you mean by stand alone mode. CYW43012 can be interfaced with host mcu through SDIO interface. It supports SDR upto 50 MHz.

Thanks

View solution in original post

0 Likes
1 Reply
Phanindra_I
Moderator
Moderator
Moderator
250 sign-ins 10 likes given 25 likes received

Hi,

Q1. They want to CYW43012 as RTOS environments not based on OS(Linux)?

>> Yes, RTOS is supported with CYW43012. You can develop applications based on RTOS for CYW43012.

Q2. Is it possible to be operated as stand alone mode?

>>  Please clarify what you mean. If you are asking about operating CYW43012 without host mcu then answer is no. The wifi applications will run on host mcu, so it cannot be operated stand alone.

Q3. If they want, they can chooose pick one method like as (WIFI only mode, BT Onlymode , WIFI & BT mode)?

>> Yes, it is possible to operate in all the mentioned modes using "WL_REG_ON", "BT_REG_ON" pins.

Q4. How fast can they transfer data?

>> Again, not sure what you mean by stand alone mode. CYW43012 can be interfaced with host mcu through SDIO interface. It supports SDR upto 50 MHz.

Thanks

0 Likes