MiniProg4 JTAG programming CYW43907

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
leaf
Level 1
Level 1
First question asked Welcome!

I'm attempting to program a CYW43907 on a custom PCB. The JTAG pins are exposed and I have the chip in boot mode. According to this it should be possible to use the MiniProg4 to program via JTAG:

https://community.cypress.com/t5/PSoC-5-3-1-MCU/Miniprog-4-JTAG/m-p/265859

According to this MiniProg4 supports the CYW43907:

https://www.cypress.com/products/psoc-programming-solutions

Yes I cannot connect. See attached screenshot.

How can I program?

(I also have a MiniProg3 which can detect the chip via a JTAG scan, however it doesn't seem to have support for a CYW43907)

 

0 Likes
1 Solution
Aditi_B
Moderator
Moderator
Moderator
500 replies posted 5 questions asked 250 replies posted

Hi,

As per the first link, MiniProg4 doesn't support program/debug via JTAG. CYW43907 supports JTAG.  MiniProg4 supports SWD.

Thanks

Aditi

View solution in original post

0 Likes
2 Replies
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

Hi @leaf  we are checking if it is feasible to program the 43907 with the miniprog4 out of the box or if some changes are necessary.

Regards, Vivek

0 Likes
Aditi_B
Moderator
Moderator
Moderator
500 replies posted 5 questions asked 250 replies posted

Hi,

As per the first link, MiniProg4 doesn't support program/debug via JTAG. CYW43907 supports JTAG.  MiniProg4 supports SWD.

Thanks

Aditi

0 Likes