Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
FrYa_4831451
Level 2
Level 2
Distributor - Weikeng(GC)
First like given 10 questions asked 10 replies posted

Hello,

I use "fqacurcy" command to set CYW4354 to transmit CW(continuous wave, non-modulated) signal, it works, but the CW signals are transmitted thru both Core0/Core1.

I tried to add "txchain" command to control it, but the CW signals are still transmitted thru both Cores.

How can I set it to transmit CW signal thru specified path?

 

Thanks for your help.

Frankie

0 Likes
1 Solution

Hi @FrYa_4831451 ,

When using the CW mode testing the power is always maximum and cannot be change, the maximum power is set by the CLM.   

View solution in original post

0 Likes
7 Replies
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

Hi @FrYa_4831451 , Could you please share us the full command list used to set continuous wave?

From the wl document link -> https://community.cypress.com/t5/Public-Archive/WL-Tool-for-Embedded-802-11-Systems-CYW43xx-Technica... the command "txchain"  take the values 1 - Chain 0 only
2 -Chain 1 only
3 -Chains 0 and 1

Could you please conform if you tried setting txchain to 1 or 2?

Regard, Vivek.

 

 

0 Likes
FrYa_4831451
Level 2
Level 2
Distributor - Weikeng(GC)
First like given 10 questions asked 10 replies posted

Hi Vivek,

The commands I used are as below:

wl down

wl mpc 0

wl txchain 1

wl up

wl band b

wl out

wl fqacurcy 1

 

Regards.

Frankie

 

0 Likes

Hi Frankie, 

-> Could you please add " txchain=1" in the NVRAM file and check if the issue still persist?

-> Does the core 0 and 1 both transmit  with  txchain 2 or 3?

Regards Vivek.

0 Likes
FrYa_4831451
Level 2
Level 2
Distributor - Weikeng(GC)
First like given 10 questions asked 10 replies posted

Hi Vivek,

 

I add the following command in NVRAM, and it can transmit the single by main path only, and I will try to modify it from "1" to "2", and check the signal can be transmitted by aux path or not.

rxchain=1
txchain=1
aa2g=1
aa5g=1

One more question, can I adjust the TX power level for this CW test by wl command?

 

Thanks.

Frankie

 

0 Likes
FrYa_4831451
Level 2
Level 2
Distributor - Weikeng(GC)
First like given 10 questions asked 10 replies posted

Hello,

Any update for TX CW power level adjusting by wl command? or it can't be supported?

 

Thanks.

Frankie

0 Likes

Hi @FrYa_4831451 ,

When using the CW mode testing the power is always maximum and cannot be change, the maximum power is set by the CLM.   

0 Likes
FrYa_4831451
Level 2
Level 2
Distributor - Weikeng(GC)
First like given 10 questions asked 10 replies posted

Hi Vivek,

Got it and thanks for your help.

Regardds.

Frankie

0 Likes