Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
yolominwoo
Level 4
Level 4
25 replies posted 10 questions asked 25 sign-ins

During the project, I need to create equipment that can be updated wirelessly using WiFi. So far, the MCU has been implemented to connect to the router. Is it possible to implement the ota upgrade with the cyw43439chip?

0 Likes
1 Solution
Aditi_B
Moderator
Moderator
Moderator
500 replies posted 5 questions asked 250 replies posted

Hi,

Currently, there is no CE included in the STM32 expansion pack to do OTA upgrade. But do visit the following CE which demonstrates an over-the-air (OTA) update with PSoC™ 6 or XMC7000 MCU and AIROC™ CYW43xxx Wi-Fi & Bluetooth® combo chips. You can try porting the same application and this can be used for OTA upgrade.

https://github.com/Infineon/mtb-example-ota-https

Thanks

Aditi 

View solution in original post

0 Likes
2 Replies
Aditi_B
Moderator
Moderator
Moderator
500 replies posted 5 questions asked 250 replies posted

Hi,

Currently, there is no CE included in the STM32 expansion pack to do OTA upgrade. But do visit the following CE which demonstrates an over-the-air (OTA) update with PSoC™ 6 or XMC7000 MCU and AIROC™ CYW43xxx Wi-Fi & Bluetooth® combo chips. You can try porting the same application and this can be used for OTA upgrade.

https://github.com/Infineon/mtb-example-ota-https

Thanks

Aditi 

0 Likes

Thank you

0 Likes