Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MaFa_974161
Level 5
Level 5
100 sign-ins 50 replies posted 50 questions asked

Hello.

I've programmed CYW954907AEVAL1F as AP to work on 120,124,128 - 5GHz Channels (Country Code IT).

I notice that it doesn't work:

with my Wi-Fi analyzer I show no AP.

 

Instead, if I program CYW954907AEVAL1F as AP to work on 36 - 5GHz Channel (Country Code IT) some Tablets doesn't connect because of "... it wasn't possibile to obtain IP addess ..."

 

 

 

0 Likes
1 Solution
raks_99
Moderator
Moderator
Moderator
First question asked 250 replies posted 250 sign-ins

Hi, 

Apologies for the delay. Is this issue resolved now? Would you like more help with it?

" it wasn't possible to obtain IP address ..."

Please make sure you are running a DHCP server like dnsmasq to assign the IP addresses.

Thanks

View solution in original post

0 Likes
3 Replies
raks_99
Moderator
Moderator
Moderator
First question asked 250 replies posted 250 sign-ins

Hi,

Can you download the test.console app by making CONSOLE_ENABLE_WL :=1 in the console.mk file
then do a wl country IT followed by wl chan_info and check if it has those channels are enabled?

Do you see channels as passive/restricted?

Thanks,

0 Likes
MaFa_974161
Level 5
Level 5
100 sign-ins 50 replies posted 50 questions asked

I write  CONSOLE_ENABLE_WL :=1 in the console.mk file

I download test.console

If I write "wl country IT" I obtain "ERROR: Unknown Command"

so I write "country IT" and processor answer "Country is (IT)".

If I write "wl chan_info" I obtain "ERROR: Unknown Command"

so I write "channel 120" and "wlog_stream on" ... the processor answer

"CONSOLE: hndarm_armr addr: 0x18011000, cr4_idx: 0
CONSOLE: 000000.000 && This is ARMCR4 core, setirqoob, coreidx: 5, flag: 13
CONSOLE: 000000.000
CONSOLE: RTE (SDIO-CDC) 7.15.168.149 (21d266a) on BCM54907 r3 @ 37.4/160.0/160.0MHz
CONSOLE: 000000.001 m2mdcdc0: Cypress M2MD CDC driver
CONSOLE: 000000.003 reclaim section 0: Returned 51232 bytes to the heap
CONSOLE: 000000.031 wl0: wlc_channels_commit: no valid channel for "#n" nbands 2 bandlocked 0
CONSOLE: 000000.032 wl0: Cypress CYW54907 802.11 Wireless Controller 7.15.168.149 (21d266a)
CONSOLE: 000000.032 TCAM: 256 used: 75 exceed:0
CONSOLE: 000000.033 reclaim section 1: Returned 92936 bytes to the heap
CONSOLE: 000000.072 wl0: wl_open
CONSOLE: 000003.073 wl0: 50 packets not freed at wlc_down. MBSS=0"

 

If I write "channel 36" and then "wlog_stream off" and then "wlog_stream on" ... the processor answer

"CONSOLE: 000000.000 && This is ARMCR4 core, setirqoob, coreidx: 5, flag: 13
CONSOLE: 000000.000
CONSOLE: RTE (SDIO-CDC) 7.15.168.149 (21d266a) on BCM54907 r3 @ 37.4/160.0/160.0MHz
CONSOLE: 000000.001 m2mdcdc0: Cypress M2MD CDC driver
CONSOLE: 000000.003 reclaim section 0: Returned 51232 bytes to the heap
CONSOLE: 000000.031 wl0: wlc_channels_commit: no valid channel for "#n" nbands 2 bandlocked 0
CONSOLE: 000000.032 wl0: Cypress CYW54907 802.11 Wireless Controller 7.15.168.149 (21d266a)
CONSOLE: 000000.032 TCAM: 256 used: 75 exceed:0
CONSOLE: 000000.033 reclaim section 1: Returned 92936 bytes to the heap
CONSOLE: 000000.072 wl0: wl_open
CONSOLE: 000003.073 wl0: 50 packets not freed at wlc_down. MBSS=0"

 

 

 

Can I have to do other ?

0 Likes
raks_99
Moderator
Moderator
Moderator
First question asked 250 replies posted 250 sign-ins

Hi, 

Apologies for the delay. Is this issue resolved now? Would you like more help with it?

" it wasn't possible to obtain IP address ..."

Please make sure you are running a DHCP server like dnsmasq to assign the IP addresses.

Thanks

0 Likes