Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos Forum Discussions

brosandic
Level 1
Level 1
First reply posted 5 sign-ins First question asked

Hi Infineon,

We are using CYW43455 chip and we want to expose command to our customers so they can decide to force 2.4GHz or 5GHz band.

wl tool documentation provides short summary about wl band command for this purposes.
However we have cases where running this command in runtime there's a kernel panic issue with following log:

[ 4461.217741] Unable to handle kernel NULL pointer dereference at virtual address 00000000
[ 4461.228950] pgd = 839ba3a3
[ 4461.233452] [00000000] *pgd=00000000
[ 4461.237061] Internal error: Oops: 5 [#1] PREEMPT SMP ARM
[ 4461.242373] Modules linked in: caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes sha256_generic libsha256 evbug brcmfmac(O) brcmutil(O) cfg80211(O) compat(O) caam error
[ 4461.260997] CPU: 0 PID: 28408 Comm: kworker/0:3 Tainted: G           O      5.10.52-0.0.004-lts-5.10.y+ #1
[ 4461.270642] Hardware name: Freescale i.MX7ULP (Device Tree)
[ 4461.276366] Workqueue: events brcmf_fweh_event_worker [brcmfmac]
[ 4461.282516] PC is at cfg80211_get_bss_channel+0xc/0x108 [cfg80211]
[ 4461.288774] LR is at cfg80211_inform_single_bss_data+0x84/0x324 [cfg80211]
[ 4461.295648] pc : [<7f0239d8>]    lr : [<7f025704>]    psr: 800f0013
[ 4461.301914] sp : 85483c88  ip : 85483d38  fp : 8564008c
[ 4461.307139] r10: 000000e3  r9 : 00000000  r8 : 85640014
[ 4461.312357] r7 : 00000000  r6 : 85483df8  r5 : 855241a0  r4 : 00000000
[ 4461.318884] r3 : 00000000  r2 : 000000e3  r1 : 8564008c  r0 : 855241a0
[ 4461.325411] Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment none
[ 4461.332543] Control: 10c5387d  Table: 65b0806a  DAC: 00000051
[ 4461.338293] Process kworker/0:3 (pid: 28408, stack limit = 0x4c154b96)
[ 4461.344814] Stack: (0x85483c88 to 0x85484000)
[ 4461.349182] 3c80:                   85483df8 855241a0 85483df8 00000000 85640014 7f025704

We were wandering what would be the right call sequence to run this command? Can we use it in runtime ?

Thanks,

Bogdan

 

0 Likes
1 Solution
Vivek_gunapati
Moderator
Moderator
Moderator
First question asked 5 likes given 250 sign-ins

Hi @brosandic  I see that this is a duplicate thread of https://community.infineon.com/t5/AIROC-Wi-Fi-and-Wi-Fi-Bluetooth/CYW43455-Correct-way-to-use-wl-ban...

Will reply to the comment in the other thread.

regards
Vivek.

View solution in original post

0 Likes
1 Reply
Vivek_gunapati
Moderator
Moderator
Moderator
First question asked 5 likes given 250 sign-ins

Hi @brosandic  I see that this is a duplicate thread of https://community.infineon.com/t5/AIROC-Wi-Fi-and-Wi-Fi-Bluetooth/CYW43455-Correct-way-to-use-wl-ban...

Will reply to the comment in the other thread.

regards
Vivek.

0 Likes
This widget could not be displayed.