- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
We have placed a CYW43439 LWB+ module from Laird on a board and are attempting to make use of both the Wi-Fi and bluetooth. We have build the backport kernel modules according to Laird documentation and are using the firmware and wpa_supplicant versions found here: https://github.com/LairdCP/Sterling-LWB-and-LWB5-Release-Packages/releases/tag/LRD-REL-10.4.0.10
We are also using the latest version of bluez.
The issue is when both Wi-Fi and Bluetooth are running simultaneously the bluetooth signal strength is terrible. So using lightblue with my phone a few feet away from my board running BLUETOOTH ONLY i see like -45dBm so pretty good. Then when i start up wpa_supplicant and it makes a connection to a network my bluetooth signal strength shoots down to -80dBm and i can't stay connected unless i am really close to the device.
I know there is one shared antenna here and the chip handles the multiplexing of both running simultaneously but something seems wrong.
The code i am using to start things up is a follows:
#STARTING BLUETOOTH
if [ ! -e "/sys/class/gpio/gpio511" ]; then
echo 511 > /sys/class/gpio/export
fi;
echo out > /sys/class/gpio/gpio511/direction
echo 0 > /sys/class/gpio/gpio511/value
sleep 3
echo 1 > /sys/class/gpio/gpio511/value
sleep 3
echo -n " Attaching bluetooth service: "
btattach -B /dev/ttyACM0 -P bcm &
hciconfig hci0 up
hciconfig hci0 leadv 0
#THEN TO START WI-FI
modprobe brcmfmac
ifplugd -i wlan0 -f -r /etc/network/ifplugdwifi.action
wpa_supplicant -i wlan0 -c /etc/wpa_supplicant.conf -Dnl80211 -B
What am i missing here? I think i am using the latest vendor provided latest version of everything at this point and still no success : /. I have attached our circuit to this as well. The chip is being powered by 3.3V, the same Rail for VBAT as well as VDDIO. I would appreciate any help or pointers i can get at this point!!!
Thanks,
Jarrod
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
Hello Anjana,
Thanks for the reply! I am using BCM4343A2_v001.003.016.0038.0000.hcd that came from the firmware package laird-lwbplus-firmware-10.4.0.10.tar.bz2 located here: https://github.com/LairdCP/Sterling-LWB-and-LWB5-Release-Packages/releases/tag/LRD-REL-10.4.0.10
Here is the output of attaching the bluetooth:
~ # btattach -B /dev/ttyACM1 -P bcm &
~ # Attaching Primary controller to /dev/ttyACM1
[ 53.872579] compat: loading out-of-tree module taints kernel.
[ 53.880393] Loading modules backported from Summit Linux version LRD-REL-9.18
[ 53.899070] Backport generated by backports.git v9.15.0.14
[ 54.025130] Bluetooth: Core ver 2.22
[ 54.032841] NET: Registered protocol family 31
[ 54.047834] Bluetooth: HCI device and connection manager initialized
[ 54.059983] Bluetooth: HCI socket layer initialized
[ 54.065254] Bluetooth: L2CAP socket layer initialized
[ 54.070678] Bluetooth: SCO socket layer initialized
[ 54.100491] Bluetooth: HCI UART driver ver 2.3
[ 54.112567] Bluetooth: HCI UART protocol H4 registered
[ 54.121685] Bluetooth: HCI UART protocol Broadcom registered
Switched line discipline from 0 to 15
Device index 0 attached
[ 54.144984] Bluetooth: hci0: BCM: chip id 147
[ 54.151906] Bluetooth: hci0: BCM: features 0x0e
[ 54.179776] Bluetooth: hci0: CYW4343A2
[ 54.183738] Bluetooth: hci0: BCM4343A2 (001.003.016) build 0000
[ 54.190153] Bluetooth: hci0: BCM4343A2 'brcm/BCM4343A2.hcd' Patch
[ 55.109952] Bluetooth: hci0: CYW43439 UART 26 MHz wlbga_BU Laird
[ 55.116295] Bluetooth: hci0: BCM4343A2 (001.003.016) build 0000
Let me know if you need any other info!
Thanks,
Jarrod
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @AnjanaM_61 ,
Did you have any thoughts or suggestions based on the above? Or some things for me to try? So far none of things i have attempted have led to any sort of success. I am using i believe all the vendor supplied software, so not sure what i could be missing here : /.
Thanks,
Jarrod
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Jarrod,
We are testing at our end and will update you in a day or two, meanwhile could you specify if any operation is performed on wifi or BT.
Regards,
Tushar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Tushar_b ,
We actually were in communications with Laird as well since they are the module supplier and it seems they too were able to recreate the issue and i believe they are currently working with you guys to resolve this issue as well!
So here is a step by step of the simplest scenario:
- Enable the BT regulator
- btattach -B /dev/ttyACM0 -P bcm &
- hciconfig hci0 up
- hciconfig hci0 leadv 0
- BLE is now advertising and i can see via Lightblue on my phone the signal strength which is good
- modprobe brcmfmac
- wpa_supplicant -i wlan0 -c /etc/wpa_supplicant.conf -Dnl80211 -B
- I have networks defined in /etc/wpa_supplicant.conf so it then connects to one that is in range
After step 8 when the wi-fi actually starts up and connects to a network the BLE signal read from lightblue drops just about off the radar, i have to be right next to the antenna to get any kind of usable bluetooth signal. If i then kill wpa_supplicant the bluetooth signal shoots back up to normal. Seems like maybe some issue with antenna multiplexing or something? Wi-Fi hogging most of the antenna time? I am not sure....
Thanks,
Jarrod
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Jarrod,
Thanks for sharing the info.
Yes, concerned S/W team is working with Laird on this issue and will update you likewise.
Regards,
Tushar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Jarrod,
Closing this thread since issue is being handled in the mycases by concerned internal team.
Regards,
Tushar