Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
JaCo_4746761
Level 1
Level 1
5 replies posted Welcome! First question asked

Hello,

We have placed a CYW43439 LWB+ module from Laird on a board and are attempting to make use of both the Wi-Fi and bluetooth.  We have build the backport kernel modules according to Laird documentation and are using the firmware and wpa_supplicant versions found here:  https://github.com/LairdCP/Sterling-LWB-and-LWB5-Release-Packages/releases/tag/LRD-REL-10.4.0.10

We are also using the latest version of bluez.

The issue is when both Wi-Fi and Bluetooth are running simultaneously the bluetooth signal strength is terrible.  So using lightblue with my phone a few feet away from my board running BLUETOOTH ONLY i see like -45dBm so pretty good.  Then when i start up wpa_supplicant and it makes a connection to a network my bluetooth signal strength shoots down to -80dBm and i can't stay connected unless i am really close to the device.

I know there is one shared antenna here and the chip handles the multiplexing of both running simultaneously but something seems wrong. 

The code i am using to start things up is a follows:

#STARTING BLUETOOTH
if [ ! -e "/sys/class/gpio/gpio511" ]; then
    echo 511 > /sys/class/gpio/export
fi;
echo out > /sys/class/gpio/gpio511/direction
echo 0 > /sys/class/gpio/gpio511/value
sleep 3
echo 1 > /sys/class/gpio/gpio511/value
sleep 3
echo -n " Attaching bluetooth service: "
btattach -B /dev/ttyACM0 -P bcm &

hciconfig hci0 up

hciconfig hci0 leadv 0


#THEN TO START WI-FI

modprobe brcmfmac

ifplugd -i wlan0 -f -r /etc/network/ifplugdwifi.action

wpa_supplicant -i wlan0 -c /etc/wpa_supplicant.conf -Dnl80211 -B

 

What am i missing here?  I think i am using the latest vendor provided latest version of everything at this point and still no success : /.  I have attached our circuit to this as well.  The chip is being powered by 3.3V, the same Rail for VBAT as well as VDDIO.  I would appreciate any help or pointers i can get at this point!!!

Thanks,

Jarrod

 

 

0 Likes
7 Replies
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hello @JaCo_4746761 ,

Can you please let us know the hcd version you are using? 

Regards,

Anjana

0 Likes
JaCo_4746761
Level 1
Level 1
5 replies posted Welcome! First question asked

Hello Anjana,

Thanks for the reply!  I am using BCM4343A2_v001.003.016.0038.0000.hcd  that came from the firmware package laird-lwbplus-firmware-10.4.0.10.tar.bz2  located here:  https://github.com/LairdCP/Sterling-LWB-and-LWB5-Release-Packages/releases/tag/LRD-REL-10.4.0.10

Here is the output of attaching the bluetooth:

~ # btattach -B /dev/ttyACM1 -P bcm &
~ # Attaching Primary controller to /dev/ttyACM1
[   53.872579] compat: loading out-of-tree module taints kernel.
[   53.880393] Loading modules backported from Summit Linux version LRD-REL-9.18
[   53.899070] Backport generated by backports.git v9.15.0.14
[   54.025130] Bluetooth: Core ver 2.22
[   54.032841] NET: Registered protocol family 31
[   54.047834] Bluetooth: HCI device and connection manager initialized
[   54.059983] Bluetooth: HCI socket layer initialized
[   54.065254] Bluetooth: L2CAP socket layer initialized
[   54.070678] Bluetooth: SCO socket layer initialized
[   54.100491] Bluetooth: HCI UART driver ver 2.3
[   54.112567] Bluetooth: HCI UART protocol H4 registered
[   54.121685] Bluetooth: HCI UART protocol Broadcom registered
Switched line discipline from 0 to 15
Device index 0 attached
[  54.144984] Bluetooth: hci0: BCM: chip id 147
[  54.151906] Bluetooth: hci0: BCM: features 0x0e
[  54.179776] Bluetooth: hci0: CYW4343A2
[  54.183738] Bluetooth: hci0: BCM4343A2 (001.003.016) build 0000
[  54.190153] Bluetooth: hci0: BCM4343A2 'brcm/BCM4343A2.hcd' Patch
[  55.109952] Bluetooth: hci0: CYW43439 UART 26 MHz wlbga_BU Laird
[  55.116295] Bluetooth: hci0: BCM4343A2 (001.003.016) build 0000

 

Let me know if you need any other info!

Thanks,

Jarrod

0 Likes
JaCo_4746761
Level 1
Level 1
5 replies posted Welcome! First question asked

Hello @AnjanaM_61 ,

Did you have any thoughts or suggestions based on the above?  Or some things for me to try?  So far none of things i have attempted have led to any sort of success.  I am using i believe all the vendor supplied software, so not sure what i could be missing here : /.

Thanks,

Jarrod

0 Likes
Tushar_b
Moderator
Moderator
Moderator
100 replies posted First like given 25 solutions authored

Hi Jarrod, 

We are testing at our end and will update you in a day or two, meanwhile could you specify if any operation is performed on wifi or BT.

Regards,

Tushar

 

 

0 Likes
JaCo_4746761
Level 1
Level 1
5 replies posted Welcome! First question asked

Hello @Tushar_b ,

We actually were in communications with Laird as well since they are the module supplier and it seems they too were able to recreate the issue and i believe they are currently working with you guys to resolve this issue as well!

So here is a step by step of the simplest scenario:

  1. Enable the BT regulator
  2. btattach -B /dev/ttyACM0 -P bcm &
  3. hciconfig hci0 up
  4. hciconfig hci0 leadv 0
  5. BLE is now advertising and i can see via Lightblue on my phone the signal strength which is good
  6. modprobe brcmfmac
  7. wpa_supplicant -i wlan0 -c /etc/wpa_supplicant.conf -Dnl80211 -B
  8. I have networks defined in /etc/wpa_supplicant.conf so it then connects to one that is in range

After step 8 when the wi-fi actually starts up and connects to a network the BLE signal read from lightblue drops just about off the radar, i have to be right next to the antenna to get any kind of usable bluetooth signal.  If i then kill wpa_supplicant the bluetooth signal shoots back up to normal.  Seems like maybe some issue with antenna multiplexing or something?  Wi-Fi hogging most of the antenna time?  I am not sure....

 

Thanks,

Jarrod

0 Likes
Tushar_b
Moderator
Moderator
Moderator
100 replies posted First like given 25 solutions authored

Hi Jarrod,

Thanks for sharing the info.

Yes, concerned S/W team is working with Laird on this issue and will update you likewise.

Regards,

Tushar

0 Likes
Tushar_b
Moderator
Moderator
Moderator
100 replies posted First like given 25 solutions authored

Hi Jarrod, 

Closing this thread since issue is being handled in the mycases  by concerned internal team.

Regards,

Tushar

 

0 Likes