As to CYW4373E SoftAP mode, is it possible to acquire the certification for the WFA (Wi-Fi Alliance) WAP3-Personal R3 ?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
PeterC
Level 1
Level 1
First reply posted First question asked Welcome!

Hi Infineon,

 

We do have a prj that planned to use CYW4373E (USB type) to work out the Wi-Fi AP feature, and the one of the mandatory is to  acquire the Wi-Fi Alliance(WFA) WPA3-Personal certification for AP mode. so the question is :

 1. We saw the data sheet of CYW4373E to show that it's to support WPA3-personal. but it doesn't show that it's to support for STA or AP mode, so the question : Is it to mean that CYW4373E supports WPA3-Personal features for AP mode ? or only to support for STA mode ? or both ? any comment ?

2. As the data sheet of CYW4373E to show that it's to support WPA3 personal, and the latest SPEC of WPA3-Personal is R3. so the question : Is the present CYW4373E supporting up to R3 ? or only R2 or earlier ? or or any comment ?

3. Is the present FW/SW/tool of CYW4373E ok to pass the test of WPA3-Personal R3 for AP mode ? if it's, can you show us where it's to download the FW/SW/tool ? or any comment ?

Thanks,

PeterC

0 Likes
1 Solution
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

Hi @PeterC , 

The latest firmware support for WPA3-R1 & WPA3-R3 in both STA as well as AP.
Driver and software releases that support WPAR3&R1 can be downloaded at the following link ->   https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2...

You can use hostapd or wpa_supplicant to configure wpa3 on AP or STA

Hope this helps
regards
Vivek.

View solution in original post

0 Likes
5 Replies
Vivek_gunapati
Moderator
Moderator
Moderator
250 replies posted 10 likes given 50 solutions authored

Hi @PeterC , 

The latest firmware support for WPA3-R1 & WPA3-R3 in both STA as well as AP.
Driver and software releases that support WPAR3&R1 can be downloaded at the following link ->   https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2...

You can use hostapd or wpa_supplicant to configure wpa3 on AP or STA

Hope this helps
regards
Vivek.

0 Likes

Hi Vivek,

 many thanks for the link, and just want to confirm if the package you provided is sufficient to pass the Wi-Fi Alliance WAP3-Personal R3 @ AP mode, that means the package is ok to acquire the WFA certified ? or NOT ?

 

Thanks,

PeterC

0 Likes

Hi @PeterC , for certification you might require to put the device in test mode. The test requires a special firmware called "MFG" or "manufacturing" firmware & .clm_blob files, these files have to be provided by the module vendor. example Murata Can you please contact your module vendor for these files?

0 Likes

Hi Vivek,

got the point, and will contact our vendor for it.

 

Thanks,

PeterC

 

0 Likes

Hi @PeterC , Since most of the queries are answered I am closing the issue, If you may have any further queries please feel free to open a new thread for further support. Thank you for choosing Infineon!

Regards
VIvek.

0 Likes