Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AIROC™ Wi-Fi MCUs Forum Discussions

AIROC™ Wi-Fi MCUs Forum Discussions

Sort by:
aniruddhann
AIROC™ Wi-Fi MCUs
Hi, I am evaluating a WiFi feature with CYW4343, using WHD driver. I see a DHCP server implemented there. And, I take it to provide IP to the station ... Show More
ecbg
AIROC™ Wi-Fi MCUs
Hello,  I try to understand the different command below and the mcs_data_rate_lookup_table. The iperf example is used to validate the modifications of... Show More
Starlord
AIROC™ Wi-Fi MCUs
Hi, We uses 'Murata Type 1LD' module which comes with pre-loaded Ayla Cloud Agent. We were wondering whether there is any way to reprogram the module ... Show More
joonbeom
AIROC™ Wi-Fi MCUs
Hi.   The below code was added to support MXIC-Memory(MX25L12835FM2I-10G) and Infineon-Memory(S25FL128LAGMFI010). ====================================... Show More
pdm
AIROC™ Wi-Fi MCUs
We have a custom PCBA similar to the CYW943907AEVAL1F.  Trying to load firmware via the JTAG port, we receive a Could not establish a connection failu... Show More
ecbg
AIROC™ Wi-Fi MCUs
Hello, I'm using two boards CYW954907AEVAL1F to transfer files using the wifi interface in mode P2P, without success. I ran all example I found in the... Show More
mtb_starter
AIROC™ Wi-Fi MCUs
Hi all,   I'm just getting started the first time with the CYW954907 and managed to run the UDP examples. However my target applications needs to use ... Show More
Starlord
AIROC™ Wi-Fi MCUs
Hi, We know that Murata Type 1LD uses two cores - Cypress and STM32. We would like to know whether WICED Studio/SDK builds a single image for both cor... Show More
KeOn_
AIROC™ Wi-Fi MCUs
I have a question about CYW43438. I don't know if GPIO_0 needs an external pullup. Please tell me the mechanism of the terminal of GPIO_0. (CMOS or op... Show More
GrCa_1363456
AIROC™ Wi-Fi MCUs
CYW943907AEVAL1F has external antenna connectors from Murata, MM8130-2600RA2 SWF microwave connector. What are some options for adapter cables or ante... Show More