AIROC™ Wi-Fi MCUs Forum Discussions
Hi,
I am a beginner. I want to configure wifi in sleep mode and wake it up as packet is received. I am using CYW43439 with STM32 controller. Can you suggest me how to proceed and what to refer in order to implement the same.
Thanks
Show LessHi Support Team
Could you provide us the most suitable SoC and Module part number for T-BOX/Smart carbody application?
It require the SOC and Module support WIFI (wifi5 is OK , no need for wifi6)+Bluetooth (classical+ble). Many thanks.
Show LessHi,
We are waiting on the serial flash support on modustoolbox for the cyw43907. Our aim is to implement OTA and also read /write some data on the flash.
Is it still planned to be implemented?
Thanks,
Cédric
Show LessHi,
How to configure wlan Sleep in CYW54907 in CYW954907AEVAL1F.
I've tried using WICED SDK and ModusToolBox for programming the device. Using Wiced Studio, I've flashed the "mfg_test" example which enables the wl tool, by which I could pass wl commands and issue the wl mpc command to put the device to sleep.
But on executing the program I came to know that it only supports the below modules,
on trying to pass commands using these exe files, the chip is not responding,
I've tried the "test_console" program from WICED studio as well, which provides a large set of commands which can be passed through any terminal programs like tera term.
There, the sleep command is not working and we are not seeing any decrease in the current numbers on issuing sleep. whereas the hibernation command is working and current numbers are decreasing as expected.
I've tried the wl43909B0.exe --serial 49 command and it is giving a response, but on issuing the mpc 1 command, I'm not seeing any decrease in the current number but the current stays at 57mA(VBAT) and 1.8mA(VDDIO).
How to use wl tool with CYW54907 for executing Sleep, transmission, etc commands.
How to put the chip in wl sleep?
please help me configure these states.
Regards,
Arun
Show LessHi ,
We meet a roaming issue: wifi disconnection happens very often.
Issue happen rate: around once per 2 hour
AP: Aruba
STA : CYW43455+RK3326
OS: Android 8
Wifi Driver: DHD
wl ver
1.363 RC125.15
wl0: Sep 26 2020 15:23:44 version 7.45.173 (r707987 CY) FWID 01-668b6f11
I find a error: TFS subelement ID unknown (65)
Is it a root cause for disconnect?
How could we fix it? or it just concerns router compatible.
Show Less
Hi,
How to measure VBAT & VDDIO currents of CYW54907 in CYW954907AEVAL1F? what modification has to be made on the board to perform the measurement?
Also How to configure the device in different WLAN Mode?
Regards,
Arun
Show LessThis was previously posted at https://community.infineon.com/t5/AIROC-Wi-Fi-MCUs/wl-tool-for-Raspberry-Pi-3-model-A/td-p/698881 but incorrectly marked as solved.
The file linked by the moderator did not work.
```
$ ./wl64 ve
./wl64: wl driver adapter not found
```
Original message:
Hi;
Where could I get the binary (or source) of the `wl` tool for a Raspberry Pi 3 (Model A+)?
```
driver: brcmfmac
version: 7.45.241
firmware-version: 01-703fd60
```
@Qi_Colin having to edit my original post because this forum is not letting me post replies (always marking them as spam)...
./wl_tool_arm64 did not work. getting the same output: ./wl_tool_arm64: wl driver adapter not found
ifconfig output:
```
$ ifconfig -a
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 44 bytes 3699 (3.6 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 44 bytes 3699 (3.6 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
wlan0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet 192.168.100.23 netmask 255.255.255.0 broadcast 192.168.100.255
inet6 2804:1e68:c60b:bd1f:da7f:58bf:f963:d00b prefixlen 64 scopeid 0x0<global>
inet6 fe80::f189:5481:8259:f74b prefixlen 64 scopeid 0x20<link>
ether xx:xx:xx:xx:xx:xx txqueuelen 1000 (Ethernet)
RX packets 351 bytes 87504 (85.4 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 254 bytes 34631 (33.8 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
```
HI,
How to connect the sensor to the CYW943907AEVALF ,please can you share any documents or code and some links , that helps me a lot.
thank you
Show Less