- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Is there a process to Load Pre-Compiled Firmware code into a CYW43xxx based kit?
Is this as simple as a MAKE command that skips the compile? "<code location> download run"
If the kit is pre-programmed to accept an OTA, the firmware can be loaded Over The Air without any special hardware .
If the kit is NOT programmed to accept an OTA is there a way to load a .hex file directly into the kit (Ideally without first purchasing a debug probe).
I understand how to program the kit using a debug probe.
I also understand how to program a kit using WICED during the compile process via a MAKE with download command.
I want to distribute pre-compiled code, to protect the IP to the extent someone can't reverse compile. Does Infineon offer a "Programmer" or "Batch File commands" that can program a WiFi kit through the kit's USB programming and debug port by using a simple USB connection to a PC?
Greg
Solved! Go to Solution.
- Labels:
-
AIROC™ Wi-Fi MCUs
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
There is no programmer supporting the CYW43907 and CYW54907. You can specify VERBOSE = 1 in the make target and see how the images are getting downloaded and try to list out the respective commands. Otherwise, you can consider using a debug probe.
Thanks,
Phanindra
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
First thing, Are you not using the wiced build system for compiling the application firmware code and doing the compilation externally. Secondly, Is the host MCU PSoC or STM based.
If it's PSoC, then there is "Cypress Programmer" that you can use for programming.
Thanks,
Phanindra
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Phanindra,
Thanks for considering my question.
First thing, Are you not using the wiced build system for compiling the application firmware code and doing the compilation externally. ==> The WICED build system could be used to create a binary file. ModusToolbox could also be used.
Secondly, Is the host MCU PSoC or STM based. ==> In my specific case, neither. I'm targeting hostless radio silicon of CYW43907 and CYW54907.
Greg
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
There is no programmer supporting the CYW43907 and CYW54907. You can specify VERBOSE = 1 in the make target and see how the images are getting downloaded and try to list out the respective commands. Otherwise, you can consider using a debug probe.
Thanks,
Phanindra