Is there a process to enable appications for CYW943907 and CYW954907 in Modus Toolbox?
Are there any instructions if there aren't any examples yet?
The kits for these two WiFi MCUs, CYW943907 and CYW954907, show up in Project Creator 1.40.
Clicking the [Next>] button for either leads to a blank screen.
After clicking [Next >]
I look forward to being able to program WiFi MCUs in ModusToolbox.
I'm specifically interested in the AT Commands associated with these parts or an explanation how Console or iPerf can perform similarly to AT Commands.
Greg
Solved! Go to Solution.
Hello Greg
We are in the process of developing CE's to be supported for xx907 devices for MTB and they should be out soon.
Thanks
Hello Greg
We are in the process of developing CE's to be supported for xx907 devices for MTB and they should be out soon.
Thanks