A peak saturated power output / ECCN / AW-CU544

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
wasu
Level 4
Level 4
Distributor - Macnica (Japan)
First like received 10 solutions authored 100 sign-ins

Hi,

Could someone tell me how to acquire "A peak saturated power output (in watts)"  for AW-CU544?

Shoudl I look into CYW43439 datasheet?

I need to know "A peak saturated power output (in watts)" to evaluate the following equation.

[Psat>505.62 W*GHz2/fGHz^2]

The above equation is from the document below.

Commerce Control List Supplement No. 1 to Part 774 Category 3—page 12

https://www.bis.doc.gov/index.php/documents/regulations-docs/2334-ccl3-8/file

b.12.a. A peak saturated power output (in watts), Psat, greater than 505.62 divided by the maximum operating frequency (in GHz) squared [Psat>505.62 W*GHz2/fGHz^2] for any channel;

 

0 Likes
1 Solution
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hello:

  I think you are asking for a max TX power at a specific frequency used on Wifi?

If this is correct, you can ask for a spec from Azurewave, they should have a fine-tuned table for TX power like 15dbm @2432M hz.

View solution in original post

0 Likes
1 Reply
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hello:

  I think you are asking for a max TX power at a specific frequency used on Wifi?

If this is correct, you can ask for a spec from Azurewave, they should have a fine-tuned table for TX power like 15dbm @2432M hz.

0 Likes