- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I havebeen struggeling with the psoc6 ble5(CM4 connected, not CM0) to get ble into sleep mode, and after that i also need to trigger theCM4 to go into sleepmode. Is there anyone that does have a simple working example, or the correct commands I need to use? I am using PSoC creator 4.4
All help is appreciated!
Ruud
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Tags:
- ble sleep
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please refer the PSoC™ 6 MCU low-power modes and power reduction techniques document for more information on lowpower modes. and also I have attached the project which works on single core CM4 .
Please let me know if this helps
Thanks
Pratiksha V
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please can you refer this code example "CE212736 - PSoC 6 MCU with Bluetooth Low Energy (BLE) Connectivity - Find Me" from PSoC Creator and also you can refer this link for API reference.
Thanks & Regards
Pratiksha V
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I did built the findme app, works great, however it uses the CM0. If I change the code to make it run on the CM4 only, it is not working anymore. I took the code of the CM0 main, and added it in the CM4-main (removed the wakeup for CM4 as that is now connected to the interrupt, en waking itself up is not what it would do). After starting the code, it take 5 mA, and does no longer function.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please refer the PSoC™ 6 MCU low-power modes and power reduction techniques document for more information on lowpower modes. and also I have attached the project which works on single core CM4 .
Please let me know if this helps
Thanks
Pratiksha V