AIROC™ Bluetooth Forum Discussions
Hey IoT Community, this is Jerry from the Bluetooth® Applications Engineering team at Infineon. We're always striving to expand available resources for our developers and part of this effort is a new webinar series called Bluetooth® Tech Lounge, an educational series geared towards both the curious and experienced to learn more about all things Bluetooth®! Our first webinar, Discovering Bluetooth® v5.4, is scheduled for December 14th and open now for registration with more topics coming in the following months. We'll be covering topics released in v5.4 such as Advertising Coding Selection, Encrypted Advertising Data, and Periodic Advertising with Responses (PAwR). Whether learning about the features for the first time or wanting a refresher on the topics, come join us next week! We hope to see you all there and looking forward to interacting with everyone to better improve the content for our developers.
AIROC™ Bluetooth® SDK 4.5.0 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.5.0.
Show LessAIROC™ Bluetooth® SDK 4.4.2 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.4.2.
Show LessAIROC™ Bluetooth® SDK 4.4.0 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW30739, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.4.0.
Show LessI want to check if CAN works with custom applications and EZ-Serial applications on the same BLE SoC. Let's say CYBT-483056.
Instead of using a separate microcontroller to send commands to the BLE SoC containing the EZ-Serial image via UART, both can be used on any CAN architecture. Suppose I have one thread running EZ serial and another thread running my application. Suppose they are communicating using some sort of function call or API that receives text or binary commands from the application thread and sends them from the EZ serial module to respond.
Show Less
AIROC™ Bluetooth® SDK 4.3.0 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW30739, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.3.0.
Show LessAIROC™ Bluetooth® SDK 4.2.1 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW30739, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.2.1.
Show LessAIROC™ Bluetooth® SDK 4.2.0 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW30739, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.2.0.
Show LessHi,
We are currently working on a project that involves the CYBT-343026-01 resp. CYW20706.
One question that came up by the market team was:
Where were the modules, and particularly the Bluetooth ICs inside the module, fabricated?
Do you share any information on that matter?
The market team highlighted that the U.S. market is currently very sensible on this topic, especially if the products are made in china.
Thanks for any help!
BR, Bernd
Show Less