Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AIROC™ Bluetooth Forum Discussions

user_ah
AIROC™ Bluetooth
hi Sir: Here is link mentioned how to incresee SPP throughout. https://community.infineon.com/t5/AIROC-Bluetooth/Increase-SPP-throughput/td-p/362635 A... Show More
MichelSole
AIROC™ Bluetooth
Hi, I am working with a CYBT-333047-02 device and we are trying to see how we can program the device going through another MCU. To explain quickly, si... Show More
KissaPeto
AIROC™ Bluetooth
Hello, We know that it is possible to disable sniff mode on CYBT-343026 module with EZserial version 1.2.38-38 by sending this command: This command ... Show More
lzc
AIROC™ Bluetooth
我按照‘Running transmitter (Tx) and receiver (Rx) sensitivity tests on CYW920829M2EVK-02’文档的描述操作时,在第三章第五步,执行double-click Reset命令后,文档描述是能收到command complet... Show More
Unknown05
AIROC™ Bluetooth

Is it possible to run Infenion AIROC bluetooth pack for configuring CY43439 without using freeRTOS (interfacing CY43439 with STM32H753)

KeTa_1341526
AIROC™ Bluetooth

Hello,

 

Does EZ-Serial Firmware use any OSS (Open Source Software) libraries or software?

 

Thanks.

hovele5678
AIROC™ Bluetooth
Dear Support Team, I am currently working on a project that utilizes the CYW20703 chip on a Windows machine. To facilitate development, I have success... Show More
hauser
AIROC™ Bluetooth
Hi,  I'm using CYW20819 and ModusToolbox and try to locate a variable at a fixed location in flash. How can I do that?   I guess I need to define a se... Show More
user_ah
AIROC™ Bluetooth
Hi Sir, There is serial flash GD25WD80CEIG on CYW920835M2EVB-01 design. Is it possible to change serial flash vendor with CYW20835 for CoB design? Is ... Show More
Tyler1
AIROC™ Bluetooth
Hi, Is the CYW89820 module designed to perform HCI_RESET at the stack level when a hardware error occurs? Also, what does Hardware Error code 0 mean?... Show More