AIROC™ Bluetooth Forum Discussions
What errata is available between CYBT-483062-02 and CYBT-483039-02?
CYBT-483039-02 appears to be end-of-life or at least NRND.
Recommended replacement appears to be CYBT-483062-02
Is CYBT-483056-02 also being promoted.
Show Less
Hi, we're doing final verification for a new product design using the CYBLE-222014-01.
I have found the intentional and unintentional radiator test reports for this device here (https://community.cypress.com/t5/Knowledge-Base-Articles/RF-Regulatory-Certifications-for-CYBLE-222005-00-and-CYBLE/ta-p/253142) but the intentional radiator report seems to be missing some tests. Test report 1622078R-RF-US-P06V02 contains:
- 15.247 (b) Maximum peak power output
- 15.247 (d) Emission on band edge
- 15.209 Radiated emissions limits (spurious emissions)
However to comply with the rules my understanding is that the following tests are also needed:
- 15.247 (a) 6dB Bandwidth
- 15.247 (e) Power spectral density
Am I incorrect in my understanding that these additional two tests are required to pass FCC? Is there any reason why these tests have not been performed?
Thanks
Show LessHi,
We have integrated CYW89820BWMLGT module with imx6ul processor and have flashed firmware.bin and minidriver.bin firmware to this chipset. We are trying to test data transfer using hcitool commands.
By executing "hcitool scan" command nearby bluetooth device will get detected but we are not able to pair and connect it. Can you please suggest us any tool which will help us for testing data transfer.
Regards,
Akshay Naik
Show LessHi, I'm looking for an electronic schematic or an application note for an infra-red remote control interface between two slot-cars and their hand controllers. It can be bluetooth, infra-red, 433MHz, or RF. It must be proporcionally linear, not simply on/off. The two hand controllers must be fully independent, operating in two different frequencies or channels.
Paulo Barbosa
Show Less
Hi Cypress.
I have some question.
How many Cypress BLE Mesh actually connection of thing?
And can you provide any refer report or test data?
Best Regard.
thank you.
Show LessHaving already worked with the TI launchpads, I expected to find a thorough several-hundred page technical reference on how the MCU in the CYBLE-013025 really works, e.g. how the devices are memory mapped into the address space, the exception model, ... . Sadly, all I could find is a brief datasheet about the module which then states that the actual silicon is a CYW20737. I couldn't find any technical reference for that MCU either! Curiously, documents in sufficient detail seem to be available for the PSoC line of chips, which makes me believe that there must also be some technical reference for the CYW20737!
Hence, my question(s):
- Where can I find the technical reference for the CYW20737?
- If no such documents exist, how is one supposed to find out about all the intricacies of the MCU?
We are using the CYW20721B2 and looking to fine tune our carrier frequency. I heard this is done, by Cypress for this part?
I may not be asking this correctly.
Other parts we use, we can set registers to select small capacitor value increments to set the carrier frequency. Not sure with this part how that is done.
Thank you,
George
Show LessGreetings, excuse the inconvenience but I have had problems with the client control mesh application, in modustoolbox, when more than 58 devices are provided in a network, it begins to present problems to open and enter more devices, I would like to know if this has any solution, in advance thanks for your time
Show Less
Does a Cypress BLE 5.0 Compatible Dongle exist to act as a central device in a USB-BLE bridge?
I am interested in the CYALKIT-E02 and the CYALKIT-E03 5 pack.
I won't need the temperature or humidity features at all. I would like to use these beacons as eddystone devices to continuously broadcast various URL's. I am wondering if these beacons will work out of the box as eddystone devices. If not, I'd like to know what it would take to get them to work as such. I see another post in the forums that seems to suggest that eddystone features are not currently working. But I also saw a note mentioning that eddystone support was added recently (in rev. B "April 2017"). If I can get these to work, I anticipate the possibility of needing dozens and eventually into the hundreds of these beacons. Is there software available to update the URL and other parameters? Will I need the E-02 kit? Can I just order the E-03 kits and get them 5 at a time without the need for the E-02 kit? These device will fit my needs beautifully if I can get them to work.
Show Less