AIROC™ Bluetooth Forum Discussions
Hi,
我比较了一下CYW920719B2Q40EVB-01和CYBT-483039-02上面的蓝牙天线电路:
CYW920719B2Q40EVB-01如下图:
CYBT-483039-02如下图:
滤波器LFB182G45CL3D178是50欧姆阻抗,贴片天线ALA321C3也50欧姆阻抗,CYW20719B2也是50欧姆阻抗。
请问:如下图所示电路是不是可以直接使用?
谢谢!
Show Less
Hello,
The data sheet for CYBT-353027-02 states that XRES has an internal resistance.
Please tell me this resistance value.
Best regards,
TK
Show LessI have an IoT project for a client where I need to connect to a phone as a BLE peripheral. While connected to the phone over BLE, I need to scan for a new connection to a Bluetooth Classic device, connect, and communicate with this device. Do any Cypress dual-mode Bluetooth modules support simultaneous BLE and Bluetooth Classic connections?
Thanks!
Brian
Show LessStep by step, according to AN91445 (Antenna Design and RF Layout Guidelines),I used HFSS to simulate the S11 parameters of MIFA antenna.The simulation results are very different from those in Figure 17.
The.brd files of MIFA for a FR4 PCB with 1.6-mm thickness are provided in the AN91445.zip file.Even when the PCB thickness (1.0-1.6mm), ground plane area (20 mm × 20 mm to 50 mm × 50 mm, Based Figure25) and L_tip, L_leg length,(Based Table3 )are adjusted as required,Results similar to Figure17 were not obtained (the best S11 data was about -5dB).COuld you provide specific PCB critical values and simulation parameters for the results in Figure17 ?
Hello,
Now, I can't reset CYW920719Q40EVB-01 by CyBluetool software. What's the problem will be?
I can Build & Download Applications via WICED Studio. Is it causing the board can't be connected with cybluetool after downloading a program by WICED Studio?
What should I do?
Show Less
Hello,
I am looking into CYW20704A2.
- What is the difference between CYW20704 and CYW20706. Can you please share link for datasheet/specifications for CYW20704A2.
- For certification related do I need to search as BCM20704 or CYW20704.
- For CYW20704 I am seeing only controller subsystem with QDID 159590 but not Host subsystem. If WICED is the support stack then what is the Host subsystem QDID.
Thanks & Regards
Vishnu Beema
@Sandeep.Suresh@Honeywell.com
Show Less您好,
请问Modus Toolbox 中如何设置CYW20719B2的Quad SPI接口?
我利用下图方法
打开了wiced_btsdk下的design.modus文件,并配置了SPI1为Quad SPI接口
SPI1工作于Slave方式。但是实际运行发现只有MOSI起作用,也就是工作于1bit方式。
请问Quad SPI该如何配置?
谢谢
Show LessHi,
Does Cypress bluetooth firmware has medical certificate?
I am interested in CYW43012 chip specifically.
Thank you.