AIROC™ Bluetooth Forum Discussions
Hello all,
I am using cyw920706 with modus toolbox successfully, that is, I can compile and install the examples 😎
But when I disable the serial flash (sw7[1-5]=off) the installation fails
How can I download directly in ram?
Show LessFor verification purpose, after CYBT-343026 goes into deep sleep mode, can we confirm the current sleep mode status via any APIs?
Hello,
programming of the device failed.
Thanks
Hi,
I have a question about Bluetooth of CYW920819EVB-02.
Is it possible to realize the functions of BT5.1 (AoA (Angle of Arraival) and AoD (Angle of Depature)) using CYW920819EVB-02?
Is there any sample code to achieve this functionality?
Is the CYW920819EVB-02 a multi-antenna?
Regards,
Sugino
I should guide RF test for the customer for CYW20706
I cannot find a RF Test tool in Modus tool.
Should I use a Cybluetool for the RF Test?
How can I enter DUT mode in that case?
If you have guide document file, Please share it
Many Thanks
Show LessHi,
I have a question about complied BT version of CY20819.
According to the datasheet CY20819 complies with BT5.0.
https://www.cypress.com/file/462851/download
However the following web site indicate CY20819 complies with BT5.2.
https://www.cypress.com/products/cyw20819
Does CY20819 support which BT versions 5.0 or 5.2?
Regards,
Nagata
What are the risks or limitations of using CYW20719B1 based radios for development while waiting for stock of new CYW20719B2 radios to become available due to current production constraints?
There is current stock of the B1 based radios at several distributors.
Stock of B2 radios is currently limited.
CYBT-483039-02 for CYBT-483056-02 - Module size: 12.75 mm × 18.59 mm × 1.80 mm
CYBT-413034-02 for CYBT-413055-02 - Module size: 12.00 mm × 16.30 mm × 1.70 mm
CYBT-423028-02 for CYBT-423054-02 - Module size: 11.00 mm × 11.00 mm × 1.70 mm
CYBT-483039-02, CYBT-413034-02 and CYBT-423028-02 are based on CYW20719B1 silicon and supported in WICED
CYBT-483056-02, CYBT-413055-02 and CYBT-423054-02 are based on CYW20719B2 silicon and supported in ModusToolbox
QDIDs are different for each
Greg
Show LessI tried to make a demo board with CYBT-343026-01 module
Actually My customer used a BM20(microchips) for the project at the moment.
They want to substitue other BT classic module because of the semiconductor shortage.
BT20 include a DAC module in it.
I wonder whether CYBT-343026-01 module has any benifit instead of BM20 or not?
If I promote CYBT-343026-01 module as substitute one. There should be some benefit in case that DAC module exist as separte module.
Many Thanks
Show Less