AIROC™ Bluetooth Forum Discussions
Hello Developer Community:
I’m using the Vela IF820 DVK (with MHF4 connector) and EZ-Serial for a serial cable replacement application using the BT Classic SPP profile. It works fine for transmitting a couple hundred bytes, but I’m losing data on the receive side when transmitting a few thousand bytes. My guess is that I’m sending data over the UART to the IF820 module faster than it can be transmitted, and overrunning some buffers. The UART configuration is 115200 8N1.
Does the IF820 module/DVK have any pins that I can monitor to gate sending data to the module before the module is ready? I’ve yet been unable to find anything useful in Laird’s documentation.
Thanks,
Matt
Show LessMay I ask how to increase the scanning distance when cyw920719b2q40evb is used as the master device, with the default configuration, it can't be scanned when it's three or four meters away
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AIROC-%E8%93%9D%E7%89%99/%E8%AF%B7%E9%97%AE%E4%B8%8B-cyw920719b2q40evb-%E4%BD%9C%E4%B8%BA%E4%B8%BB%E8%AE%BE%E5%A4%87%E7%9A%84%E6%97%B6%E5%80%99-%E5%A6%82%E4%BD%95%E6%8F%90%E9%AB%98%E6%89%AB%E6%8F%8F%E8%B7%9D%E7%A6%BB/td-p/496263
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AIROC-%E8%93%9D%E7%89%99/CYW89829-%E4%B8%93%E7%94%A8ADC%E9%97%AE%E9%A2%98/td-p/723824
Show LessHi Sir,
How to set the CYW20835 LE tx power?
Firmware I use the "Empty BTSDK App" generated by ModusToolbox .
I tried to use bluetool to send "Write Tx Power Table" command to "HCI UART" but the response is "Unknown HCI Command".
I used CYW20704 to test the "Write Tx Power Table" command response and it was OK.
Show Less
Bluetooth-LE Audio に対応したチップを探しています。
対象チップを紹介頂けないでしょうか。
Hi,
I am trying to understand why calling
wiced_bt_set_local_bdaddr
and/or just calling and printing out the BDA address through
wiced_bt_dev_read_local_addr( bda );
Does not match up to the BLE Address I see in CySmart for the chip or with Light Blue.
Each time I reboot the device , Light Blue will change the address it is seeing, but it never matches what I try to set it to. If I call the set and read they match, but it does not appear to set the BDA that is actually being broadcast.
What I am setting up wrong?
I have proven this with both my code and with Hello_Sensor
Show Less
Dear everyone
Customer need to build the CYW20707 footprint, but they found the pin name is different from Ball Map.
Because customer request two part need to be consistent.
Will Infineon revise the document?
Or can customer use Ball Map name as a focus first?
The difference list as attached file.
Thank you.
Show LessHi, we would like to design a bluetooth wireless microphone for singers. We found out this module CYBT-343026-01 and we think it could be fit our needs. We also found a repo here https://github.com/Infineon/mtb-example-btsdk-audio-handsfree with an useful example. The problem is that this example is made for CYW920721M2EVK-02 target, so is it possible to change the target in order to use our module which is the CYBT-343026-01? If not, can you suggest us any idea to start using HFP for voice transmission with CYBT-343026-01. Thank you.
Show LessI am using CYW920706WCDEVAL's audio Headset app on CYBT-343026-EVAL (CYBT-343026-01) board. I have implemented the changes in Makefile and also added the CYBT-343026-EVAL file in deps folder. but still it is showing error "Too many patch entries for device"
Building application =
==============================================================================
Generating compilation database file...
-> ./build/compile_commands.json
Compilation database file generation complete
Generated 1 source file(s)
C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/generated/lib_installer.c already present, use clean if it needs updating
Building 34 file(s)
Compiling C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/generated/lib_installer.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/sparinit.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/wiced_bt_app_common.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/wiced_bt_app_hal_common.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0/platform.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile/wiced_bt_a2dp_m12.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/generated/lib_installer.c:47:2: error: #error Too many patch entries for device, after adding libraries
47 | #error Too many patch entries for device, after adding libraries
| ^~~~~
make[1]: *** [../mtb_shared/core-make/release-v1.9.1/make/core/build.mk:382: C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/Debug/generated/lib_installer.o] Error 1
make[1]: *** Waiting for unfinished jobs....
make: *** [../mtb_shared/core-make/release-v1.9.1/make/core/main.mk:434: secondstage_build] Error 2
"C:/Users/27305/ModusToolbox/tools_3.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=3.2 CY_IDE_TOOLS_DIR=C:/Users/27305/ModusToolbox/tools_3.2 -j8 all" terminated with exit code 2. Build might be incomplete.
I am a beginner. I am Trying to implement handsfree profile using CYBT-243053 EVAL - 01 (standalone project). I have configured bluetooth using bluetooth configurator in Modus Toolbox. But how to add functions for this configurations. Or any hint from where i can take reference for creating HFP using CY-BT243053.
Thanks....
Show Less