AIROC™ Bluetooth Forum Discussions
Hi,
I am trying to understand why calling
wiced_bt_set_local_bdaddr
and/or just calling and printing out the BDA address through
wiced_bt_dev_read_local_addr( bda );
Does not match up to the BLE Address I see in CySmart for the chip or with Light Blue.
Each time I reboot the device , Light Blue will change the address it is seeing, but it never matches what I try to set it to. If I call the set and read they match, but it does not appear to set the BDA that is actually being broadcast.
What I am setting up wrong?
I have proven this with both my code and with Hello_Sensor
Show Less
I just got the development board and learned the schematics and hardware debugging of the cyw920820.
I want to download the program directly to the cyw20820 chip through swd, and I access SWCLK, SWDIO and GND pins through the fly wire.
I followed the tutorial to modify ENABLE_DEBUG=1 in the makefile. I know that the chip does not define the SWD pin by default, so I see in spar_utils.h that the macro definition sets SWD.
There are a few questions
1. I changed ENABLE_DEBUG=1 in the makefile. Why is this area still undefined in my spar_utils.h diagram?
2. Set the parameters in the preceding method, but the download fails. The following message is displayed, indicating that the hardware has been connected for many times,The relevant SW switch has been turned off on the development board
3. I see AIROC-hardware-debug says BUSY_WAIT_TILL_MANUAL_CONTINUE_IF_DEBUG_ENABLED(). After ENABLE_DEBUG=1, do I need to adjust anything。#cyw20820
Currently, I put SETUP_APP_FOR_DEBUG_IF_DEBUG_ENABLED(). BUSY_WAIT_TILL_MANUAL_CONTINUE_IF_DEBUG_ENABLED() placed in the application_init function
makefile ENABLE_DEBUG?=1
Show Less
I am using the chip cyble222014 to test Bluetooth communication, currently using mini program4 5pin port to program but it says Psoc device is not acquired, I have carefully checked the connection everywhere, so anyone understand how it is,what is wrong, thank you very much
Show LessAIROC™ Bluetooth® SDK 4.6.3 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835B1, CYW20819, CYW20820, CYW20829, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.6.3.
Show LessHi Infineon team,
We are facing some issue when migrating from the development board to integrating the module on to our own platform.
The issues we face are,
1. When in the 'application' mode, the UART interface is communicating at a baud rate of 137.3626 kbps, which is different from the standard baud rate we had found in the evaluation board of 115.2 kbps.
2. We have not gained full understanding of the 'Recover' mode of the Bluetooth module. Would you be elaborate what the 'Recovery' button does and if a connection to MOSI pin is required for our platform?
Kind regards,
Remo
Show Less
While running Hello World example in cyw920829m2evk-02 kit using Eclipse Modus Toolbox IDE the code sucessfully gets programmed but does not work. While analysing noticed that in cycfg_pins.h file, the configuration pins are disabled,tried out other examples similar issue is faced.
Show LessThe project uses 6-10 burners in parallel, to burn at the same time Now found that can not be burned at the same time, only a single burner found that can be burned at the same time burner are 17/18, can not be burned at the same time burner is the beginning of 21
Does this have anything to do with version? Is there a version requirement for parallel use?
If it's a version issue , what was updated at the beginning of 21?
Please help with the answer!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-Creator-Designer/CY8CKIT-002-%E7%83%A7%E5%BD%95%E5%99%A8%E8%BF%87%E7%A8%8B%E4%B8%AD%E7%9A%84%E4%B8%8D%E8%83%BD%E5%90%8C%E6%97%B6%E7%83%A7%E5%BD%95%E7%9A%84%E9%97%AE%E9%A2%98/td-p/712855
Show Lessgetting error
Break at address "0x50dc3e" with no debug information available, or outside of program code. if i debug using OpenOCD and cable used is kitprog3 (provided with the board).
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
[CYW20820A1.cpu] halted due to debug-request, current mode: Thread
xPSR: 0x61000000 pc: 0x0050dc42 psp: 0x00227670
Warn : Prefer GDB command "target extended-remote :3333" instead of "target remote :3333"
===== arm v7m registers
AIROC™ Bluetooth® SDK 4.6.2 is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20736, CYW20835, CYW20819, CYW20820, CYW89820, CYW43012 AIROC™ Wi-Fi & Bluetooth® combo chips (for embedded Bluetooth® development only), and CYW5557x AIROC™ Wi-Fi & Bluetooth® combo chips. ModusToolbox™ software with the Bluetooth® SDK software library provides a complete development environment to allow you to quickly create Bluetooth®-enabled IoT solutions such as smartwatches, medical devices, or home automation platforms. This document describes the features and known limitations of Bluetooth® SDK 4.6.2.
Show LessHi, I am a beginner trying to implement HFP (for calls) using CYW920820M2EVB-01 as standalone project by Modus Toolbox. Does this board supports HFP as no example code is given for the respective board related to HFP.
Show Less