Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AIROC™ Bluetooth Forum Discussions

Sort by:
joshm
AIROC™ Bluetooth
I have a project that is based off DFU_BLE_Upgradable_Stack (CE220960), and I have made a few adjustments to make the the projects to work with PDL v3... Show More
NXTY_Shibutani
AIROC™ Bluetooth
静電気試験にて、マイコンが停止したまま復帰しない(GPIO/BLEともに出力しない)現象が発生しています。調査を進めた結果、I2C通信ラインへのノイズによる影響ではないかと考えております。 I2C通信ライン自体のノイズ耐性を向上させることは可能でしょうか?(ハードウェアorソフトウェア)フィルタの追... Show More
Communication
AIROC™ Bluetooth
Xin chào! Tôi đang xây dựng một dự án sử dụng PSoC 63 BLE và Modustoolbox để đọc dữ liệu từ các cảm biến và sử dụng Bluetooth để truyền dữ liệu qua mộ... Show More
KeOn_
AIROC™ Bluetooth
Hi,I can't reply to the thread below, so I'm creating a new question.https://community.infineon.com/t5/AIROC-Wi-Fi-and-Wi-Fi-Bluetooth/CYW4373E-Hang-up-of-farmware/m-p/393706/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExDWlpUU1BYVkNJMEZCfDM5MzcwNnxTVUJTQ1JJUFRJT05TfGhL#M1912... Show More
eyurko
AIROC™ Bluetooth
Hello,    I am working with the 202007 BLE module and I have an external antenna connected to the uconnector and am receiving signal strength of -80dB... Show More
PrN_4452166
AIROC™ Bluetooth
Hi Team I am looking for an alternative to a Bluetooth module (PN: BT121 @ Silicon Labs).  Our Requirements are:  1. It should support both BLE and Bl... Show More
jbruneaux
AIROC™ Bluetooth
Hi, For our product under development, we need to implement some basic tests commands, and I've been able to implement the Set_Tx_Carrier_Frequency_AR... Show More
jbruneaux
AIROC™ Bluetooth
Hi, We are experiencing unexpected reboot of a CYBT-483056-02 module used on a CYBT-403056-EVAL board under some circumstance (two connection created)... Show More
And_
AIROC™ Bluetooth
Hi,  Because of the standard Serial Port Profile (SPP) is not supported by BLE, i need to create a BLE custom service to be able to send/receive UART ... Show More
seanb
AIROC™ Bluetooth
Hi Community, I'm using PSoC 62 with LBEE5KL1DX (with CY4343W). The advertisement name comes from the Bluetooth Configurator's GAP settings. But becau... Show More