AIROC™ Bluetooth Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
I'm working with a distribution partner and the customer to figure out a method to interface with an eMMC using the BLE module CYW20829B0-P4TAI100. The purpose is for data logging.
Can you please advise if it's possible to interface with an eMMC memory using the QSPI peripheral?
Regards,
Marcelo - FAE at Neutronics
Show LessHey
Can i get a sample project to do a2dp sink for the CYW20820
/Peter
Is there a command for directly controlling CYBLE-212006-01 through a serial port?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AIROC-%E8%93%9D%E7%89%99/Testing-of-CYBLE-212006-01/td-p/501646
Show Lessmy board is CYW20829
When I was writing my BLE program based on RTOS, I created some other tasks and ran the program, which caused Bluetooth to fail to initialize, meaning it could not start. The program only printed the content before Bluetooth initialization.
/* Initialize bluetooth porting layer by setting HCI configuration */
cybt_platform_config_init(&cybsp_bt_platform_cfg);
/* Register call back and configuration with stack */
result = wiced_bt_stack_init(app_bt_management_callback,
&wiced_bt_cfg_settings);
/* Check if stack initialization was successful */
if( WICED_BT_SUCCESS == result)
{
printf("Bluetooth Stack Initialization Successful \n");
}
else
{
printf("Bluetooth Stack Initialization failed!! \n");
CY_ASSERT(0);
}
The program printed Bluetooth Stack initialization successfully on the terminal, but it seems that the program is stuck in a certain task, causing Bluetooth to not start properly and not complete the broadcast. I would like to ask what direction I should take to solve this problem when it arises. (Note: I modified it using the modustoolbox BLE routine). In other words, under what circumstances will Bluetooth fail to start
Show LessMay I ask how to increase the scanning distance when cyw920719b2q40evb is used as the master device, with the default configuration, it can't be scanned when it's three or four meters away
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AIROC-%E8%93%9D%E7%89%99/%E8%AF%B7%E9%97%AE%E4%B8%8B-cyw920719b2q40evb-%E4%BD%9C%E4%B8%BA%E4%B8%BB%E8%AE%BE%E5%A4%87%E7%9A%84%E6%97%B6%E5%80%99-%E5%A6%82%E4%BD%95%E6%8F%90%E9%AB%98%E6%89%AB%E6%8F%8F%E8%B7%9D%E7%A6%BB/td-p/496263
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AIROC-%E8%93%9D%E7%89%99/CYW89829-%E4%B8%93%E7%94%A8ADC%E9%97%AE%E9%A2%98/td-p/723824
Show LessBluetooth-LE Audio に対応したチップを探しています。
対象チップを紹介頂けないでしょうか。
Hi, we would like to design a bluetooth wireless microphone for singers. We found out this module CYBT-343026-01 and we think it could be fit our needs. We also found a repo here https://github.com/Infineon/mtb-example-btsdk-audio-handsfree with an useful example. The problem is that this example is made for CYW920721M2EVK-02 target, so is it possible to change the target in order to use our module which is the CYBT-343026-01? If not, can you suggest us any idea to start using HFP for voice transmission with CYBT-343026-01. Thank you.
Show LessI am using CYW920706WCDEVAL's audio Headset app on CYBT-343026-EVAL (CYBT-343026-01) board. I have implemented the changes in Makefile and also added the CYBT-343026-EVAL file in deps folder. but still it is showing error "Too many patch entries for device"
Building application =
==============================================================================
Generating compilation database file...
-> ./build/compile_commands.json
Compilation database file generation complete
Generated 1 source file(s)
C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/generated/lib_installer.c already present, use clean if it needs updating
Building 34 file(s)
Compiling C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/generated/lib_installer.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/sparinit.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/wiced_bt_app_common.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/wiced_bt_app_hal_common.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0/platform.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
Compiling ../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile/wiced_bt_a2dp_m12.c -DWICED_BT_TRACE_ENABLE -DAVRC_ADV_CTRL_INCLUDED -DAVRC_METADATA_INCLUDED -DWICED_BT_HFP_HF_MAX_CONN=2 -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=1000000 -DHCI_UART_DEFAULT_BAUD=115200 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYBT_343026_EVAL"' -DCYBT_343026_EVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYBT_343026_EVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_avrc_controller -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCOMPONENT_handsfree_profile -DCY_SUPPORTS_DEVICE_VALIDATION -DCYBT_343026_02 -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYBT-343026-EVAL/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.5.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v4.5.1/COMPONENT_handsfree_profile -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v4.5.1/include -I./handsfree -I./remote_controller
C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/generated/lib_installer.c:47:2: error: #error Too many patch entries for device, after adding libraries
47 | #error Too many patch entries for device, after adding libraries
| ^~~~~
make[1]: *** [../mtb_shared/core-make/release-v1.9.1/make/core/build.mk:382: C:/Users/27305/mtw/Audio_Headset/build/CYBT-343026-EVAL/Debug/generated/lib_installer.o] Error 1
make[1]: *** Waiting for unfinished jobs....
make: *** [../mtb_shared/core-make/release-v1.9.1/make/core/main.mk:434: secondstage_build] Error 2
"C:/Users/27305/ModusToolbox/tools_3.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=3.2 CY_IDE_TOOLS_DIR=C:/Users/27305/ModusToolbox/tools_3.2 -j8 all" terminated with exit code 2. Build might be incomplete.