AIROC™ Bluetooth Forum Discussions
Hi,
Does EZ-serial FW(CYBT-343026/CYBT-343151 module) support advertisig forever command??
if so. how to configure command for advertisig forever command?
Thanks.
Austin
Show LessHi,
What's the life cycle status on CYW20706? I've noticed that CYW20706 isn't listed under AIROC™ Bluetooth® LE & Bluetooth® any more. Mouser is now also listing the part as not recommended for future design.
What would be a good replacement part for the CYW20706. And will there likely be a dual stack Bluetooth SoC that also supports LE Audio?
Thanks.
Regards,
Tong
Show LessDear Infineon,
1. The CYW20736 sleep current is 13uA(datasheet max.), can I know the deep sleep current?
2. The battery is expected to be L91 or EL123AP. Can I refer to any relevant document or calculation tool for battery life estimation? For example, what is the connection mode time and current consumption? Advertising or scan time and current?
Thanks.
Show LessHi
我正在学习pawr_lelr这个文件,目前有个疑问:makefile中DEMO_SET ?=0的作用是什么?
请问89820/ mcu可以开放给客户二次开发吗?有什么限制?
We are using the EZ-serial firmware V1.2.36 of the CYBT-343026-01 module. After power on of the module I use an android device to connect to the BLE peripheral interface for Unacknowledged data. Connection succeeds, but serial data is not forwarded to the BLE connection unless ~50 seconds has passed or a full 20 characters are sent. The packetization mode is Anticipate (1) with default parameters (5 ms, 20 characters). What could be causing this 50 second delay? Its almost as if the 5 ms timer is not expiring.
I can send data on the BLE connection and it is transmitted on the serial interface immediately.
After waiting the 50 seconds after power on then serial data is transferred over BLE without delay.
If I change the packetization mode to Immediate (0) then the serial data is passed to the BLE connection with no delay.
Ed
Show LessHi,
Rightnow, I'm using cybt-213043-mesh to transmit temperature to PC. And I'm only using 1 code "Mesh_Demo_Temperature_Sensor". For low power node, I set up with "LOW_POWER_NODE ?= 1" (low power node) in makefile. But the current consumption of low power node is still too high.
My question is what is the optimal setup of "Mesh_Demo_Temperature_Sensor" beside "LOW_POWER_NODE ?= 1" to reduce the current consumption of low power node as low as possible.
Thank,
Show LessHi,
I am verifing EZ-Serial WICED Firmware with customized characteristic. I refer "3.6.4 Notifying and Indicating Data to a Remote Client" in doc Infineon-EZ-Serial_WICED_Firmware_Platform_User_Guide_for_CYW2070x-based_Modules-ReferenceDesign-v02_00-EN.pdf.
But those command in user gudie didn't work well. have you more example command to create customized characteristic for read/write/notify/indicated?
Thanks.
Austin
Show LessHello,
I am working on updating the EZ-Serial Module Firmware over OTA for the CYBT-343026 device. I'm using the image from CYBT-343026-01-EZ-Serial_v1.2.38.0.zip
. I noticed that there are both .bin and .hex files available. While I was able to use the .bin file, I couldn't use the .hex file. Could you please explain the purpose of the .hex file?
Thank you in advance for your assistance.
Best regards,
Kazuki
Show Less