Starting with Modus Toolbox SDK.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
TDC
Level 1
Level 1
First solution authored 10 sign-ins 5 replies posted

Hello @DheerajPK_41 ,

I have installed Modus Toolbox v2.4, i want to use CYBT-413034_02. I have successfully installed the IDE, when I create a New application, in project creator I couldn't find CYBT-413034_02 BSP, so I tried to use  CYW920719B2Q40EVB-01 and created a RFCOMM project. While downloading, the serial port is not detecting, i tried to put it into recovery mode, still no luck.

I even tried to make a custom BSP, with the help of this link https://community.infineon.com/t5/Knowledge-Base-Articles/ModusToolbox-2-2-and-later-Make-a-Custom-B...

I didn't understood this point, which directory should I select?

Go to the top level of your new application directory where the makefile is located and use the make bsp command.

i change the directory location to this, and change my folder name to TARGET_MyBSP

\mtw\mtb_shared\wiced_btsdk\dev-kit\bsp

make bsp TARGET_GEN=MyBSP DEVICE_GEN=CYBT_413034-02

I am getting error as make: *** No rule to make target 'bsp'. Stop.

Thank You

 

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

CYBT_413034-02 is bit old module based on CYW20719B1 chip which will not be supported in Modustoolbox. You can try getting the latest module based on CYW20719B2 to work with Modustoolbox. 

Eg. CYBT-413054, CYBT-413055

Thanks,

-Dheeraj.P.K

View solution in original post

0 Likes
3 Replies
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

CYBT_413034-02 is bit old module based on CYW20719B1 chip which will not be supported in Modustoolbox. You can try getting the latest module based on CYW20719B2 to work with Modustoolbox. 

Eg. CYBT-413054, CYBT-413055

Thanks,

-Dheeraj.P.K

0 Likes

Hello @DheerajPK_41 ,

Are  CYBT-413054, CYBT-413055 are pin compactible with CYBT-413034?

 CYBT-413061 is available rather than  CYBT-413054?

Thank You.

0 Likes
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Update:

Compatible. Please have a look at the Schematic from the below page.

https://www.infineon.com/cms/en/product/wireless-connectivity/airoc-bluetooth-le-bluetooth-multiprot...

 

 CYBT-413061 is CYW20721 module and CYBT-413054 is CYW20719 module. Both are available. 

Please contact our sales/marketing team.

0 Likes