- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm using a CYBLE222014-01, and need to optimize the battery use. I have two questions about hibernate mode:
1. There is conflicting documentation about the wakeup time:
- The datasheet (PRoC™ BLE: CYBL1XX7X Family Datasheet, 001-95464 Rev. *K) says on page 22 the wakeup time is 0.7 ms.
- The AppNote (AN92584 Designing for Low Power and Estimating Battery Life for BLE Applications) says on page 3 the wakeup time is 2 ms.
Which document is right?
2. During this ambiguous wakeup time, the processor is transitioning from hibernate (150nA) to active mode (13,400,000nA). This has obvious effects on the power budget. What is the current consumption during the transition? Which figure should I use?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
We don't have any power spec for this transition time. It might be the transition time to active mode so the current should ideally increase to active current.
The delays at the startup code is to allow various clocks to settle. The device will be in active mode during this time.
Thanks,
P Yugandhar.