Is there an example of BLE OTA bootloader with MTB? If not what is the best way to construct that?
I see this DFU, but it does not support BLE as a transport.
https://github.com/Infineon/mtb-example-psoc6-dfu-basic
Solved! Go to Solution.
Hi @Panometric
Please refer to the attached project, where firmware update happens via BLE. Please refer README file for more information.
Please let me know if this helps.
Thanks & Regards,
Pratiksha V
Hi @Panometric
I would suggest you to go through PSoC 6 MCU BLE Upgradable Stack Bootloader example project available in our PSoC creator IDE as reference for creating an example in Modustoolbox.
https://www.infineon.com/cms/en/search.html#!term=CE220960&view=all
Regards,
Pratiksha V
@PratikshaV We need a solution that works in MTB.
Q1: Are you suggesting I build the BLE bootloader and Launcher in Creator and import it into MTB like AN219434?
I'm trying the examples, Using PsocCreator 4.2 with PDL 3.0.1 like other posts say.
Q2: Should the export to MTB 2.4 be Eclipse CMSIS or Make based, since it is both?
Q3: I tried exporting a makefile IDE for App1, and I get this error:
Hi @Panometric
you cannot directly import the above example from Psoc creator to MTB like AN219434 you can just take it as a reference for more information on firmware update you can refer the below link
https://infineon.github.io/dfu/dfu_sdk_api_reference_manual/html/index.html#group_dfu_ucase_ble
Please let me know if this helps
Thanks & Regards
Pratiksha V
@PratikshaV It helps a little. You are suggesting that all the time I spent trying to
CE220960 to work was a waste and that I should be using the DFU 4.2 method.
This procedure is quite involved and only designed for boards I do not have, even though I own 3 different Psoc6 boards. Given my past experience, I'm doubtful I could have it working in a few hours. In addition, it refers back to CE216767 which is in Creator which is confusing. Has the BLE path been tested ? If so, why not provide the tested projects as an example instead of https://github.com/Infineon/mtb-example-psoc6-dfu-basic
?
Furthermore the DFU 4.2 instructions do not appear to support a Shared BLE stack application which will be very important for a smaller memory device. Is it as simple as just enabling "OTA Bootloading and Code Sharing" in the device configurator?
https://infineon.github.io/dfu/dfu_sdk_api_reference_manual/html/index.html#group_dfu_mtb_cfg
Note: I tried DFU 4.2 QSG , and got hit a mistake on 1.4: "Copy folder from ..\mtb_shared\TARGET_[KIT_NAME]\[VERSION]\COMPONENT_BSP_DESIGN_MODUS to the project root and rename it to DFU_DESIGN_MODUS." because my mtb-shared directory has no folders like "TARGET_*" nor does it have any file named "COMPONENT_BSP_DESIGN_MODUS". Those are in the projects directory, not the shared directory. I think what they meant to say was to create COMPONENT_CUSTOM_DESIGN_MODUS folder and edit the peripherals there.
Hi @Panometric
Please refer to the attached project, where firmware update happens via BLE. Please refer README file for more information.
Please let me know if this helps.
Thanks & Regards,
Pratiksha V