cancel
Showing results for 
Search instead for 
Did you mean: 

AIROC™ Bluetooth

tado_4837711
New Contributor II

Hi Community:

We are now use CYBT_343026_EVAL (WICED-SDK Version: Wiced_006.004.000.0061) working as a Dual-mode Bluetooth controller with LL Privacy enabled.

When doing the LE_Create_Connection with Own_Address_Type = 0x3(3, "RPA or Random Address") , the controller always HCI Command Complete Event with Status = 0xC (12, "Command Disallowed", "Command Disallowed"). 

Below is the HCI log:

tado_4837711_0-1631674632355.png

We also did a simple test with Cybluetool :

09/14/21 13:01:07.460 com3@115200 c> Reset
HCI Command
com3@115200
[03 0C 00 ]
opcode = 0x0C03 (3075, "Reset")


09/14/21 13:01:07.467 com3 <c Reset
HCI Command Complete Event
com3@115200
[0E 04 ]: 01 03 0C 00
event = 0x0E (14,"Command Complete")
Num_HCI_Command_Packets = 0x1 (1)
Command_Opcode = 0xC03 (3075, "Reset")
Status = 0x0 (0, "Success", "Success")


09/14/21 13:01:39.941 com3@115200 c> LE_Read_Local_Supported_Features
HCI Command
com3@115200
[03 20 00 ]
opcode = 0x2003 (8195, "LE_Read_Local_Supported_Features")


09/14/21 13:01:39.946 com3 <c LE_Read_Local_Supported_Features
HCI Command Complete Event
com3@115200
[0E 0C ]: 01 03 20 00 FF 00 00 08 00 00 00 00
event = 0x0E (14,"Command Complete")
Num_HCI_Command_Packets = 0x1 (1)
Command_Opcode = 0x2003 (8195, "LE_Read_Local_Supported_Features")
Status = 0x0 (0, "Success", "Success")
LE_Features = "FF 00 00 08 00 00 00 00"


09/14/21 13:02:07.445 com3@115200 c> LE_Create_Connection
HCI Command
com3@115200
[0D 20 19 ]: 64 00 32 00 00 00 11 11 11 11 11 11 03 02 00 02 00 00 00 0A 00 00 00 00 00
opcode = 0x200D (8205, "LE_Create_Connection")
LE_Scan_Interval = 0x64 (100, in slots. Range: 2.5ms to 10.25s)
LE_Scan_Window = 0x32 (50, in slots. Range: 2.5ms to 10.25s)
InitiatorFilterPolicy = 0x0 (0, "White List not used and the Peer address in this command is used")
Peer_Address_Type = 0x0 (0, "Public Address")
Peer_Address = "111111111111"
Own_Address_Type = 0x3 (3, "RPA or Random Address")
Conn_Interval_Min = 0x02 (2)
Conn_Interval_Max = 0x02 (2)
Conn_Latency = 0x00 (0)
Supervision_Timeout = 0x0A (10)
Minimum_CE_Len = 0x00 (0, in slots. Range:1 to 2*Conn_Interval)
Maximum_CE_Len = 0x00 (0, in slots. Range:1 to 2*Conn_Interval)


09/14/21 13:02:07.451 com3 <e Command Status
HCI Event
com3@115200
[0F 04 ]: 0C 01 0D 20
event = 0x0F (15,"Command Status")
Status = 0xC (12, "Command Disallowed", "Command Disallowed")

Please support us do a kind check  on this issue?

 

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator

Hi,

As per the spec, the controller shall return "Command Disallowed (0x0C)" error code If the Host issues HCI_LE_Create_Connection command when another HCI_LE_Create_Connection command is pending in the Controller.  Please confirm it is not so in your testing.

I could also reproduce similar issue. We will check this with our firmware team. 

 

Could you please let us know the scenario where you uses Own_Address_Type = 0x3 (3, "RPA or Random Address")?

 

Thanks,

-Dheeraj.P.K

View solution in original post

0 Likes
6 Replies
AnjanaM_61
Moderator
Moderator

Hello @tado_4837711 

I don't see 'scan enable ' before creating a connection. Can you please make sure to enable scan and then try connecting to the peer device?

Thanks,

Anjana

0 Likes
tado_4837711
New Contributor II

I did not do the scan enable because of we know the remote peer device‘s address。 

As you suggested, also tried with scan enable,still "Command Disallowed" when LE_Create_Connection with  Own_Address_Type = 0x3 (3, "RPA or Random Address")

09/16/21 08:52:04.706 com3@115200 c> Reset

HCI Command

com3@115200

[03 0C 00 ]

opcode = 0x0C03 (3075, "Reset")

 

 

09/16/21 08:52:04.715 com3 <c Reset

HCI Command Complete Event

com3@115200

[0E 04 ]: 01 03 0C 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0xC03 (3075, "Reset")

Status = 0x0 (0, "Success", "Success")

 

 

09/16/21 08:52:12.019 com3@115200 c> LE_Read_Local_Supported_Features

HCI Command

com3@115200

[03 20 00 ]

opcode = 0x2003 (8195, "LE_Read_Local_Supported_Features")

 

 

09/16/21 08:52:12.025 com3 <c LE_Read_Local_Supported_Features

HCI Command Complete Event

com3@115200

[0E 0C ]: 01 03 20 00 FF 00 00 08 00 00 00 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x2003 (8195, "LE_Read_Local_Supported_Features")

Status = 0x0 (0, "Success", "Success")

LE_Features = "FF 00 00 08 00 00 00 00"

 

 

09/16/21 08:52:27.219 com3@115200 c> LE_Set_Scan_Enable

HCI Command

com3@115200

[0C 20 02 ]: 01 01

opcode = 0x200C (8204, "LE_Set_Scan_Enable")

LE_Scan_Enable = 0x1 (1, "Scanning is enabled")

Filter_Duplicates = 0x1 (1, "Duplicate filtering is enabled")

 

 

09/16/21 08:52:27.224 com3 <c LE_Set_Scan_Enable

HCI Command Complete Event

com3@115200

[0E 04 ]: 01 0C 20 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x200C (8204, "LE_Set_Scan_Enable")

Status = 0x0 (0, "Success", "Success")

 

 

09/16/21 08:52:27.233 com3 <e LE Event

HCI Event

com3@115200

[3E 26 ]: 02 01 00 01 BC B4 5B C1 99 6D 1A 02 01 1A 02 0A 08 13 FF 4C 00 0C 0E 00 73 49 56 A4 95 6E F5 17 86 5B 6A B8 68 AC

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "6D99C15BB4BC"

Data_Len[0] = 0x1A (26)

Data[0] = "02 01 1A 02 0A 08 13 FF 4C 00 0C 0E 00 73 49 56 A4 95 6E F5 17 86 5B 6A B8 68"

RSSI[0] = 0xAC (-84, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.268 com3 <e LE Event

HCI Event

com3@115200

[3E 1E ]: 02 01 00 01 A5 88 4F DD 24 69 12 02 01 1A 02 0A 0C 0B FF 4C 00 10 06 5A 1E 7D 4C 80 44 BE

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "6924DD4F88A5"

Data_Len[0] = 0x12 (18)

Data[0] = "02 01 1A 02 0A 0C 0B FF 4C 00 10 06 5A 1E 7D 4C 80 44"

RSSI[0] = 0xBE (-66, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.290 com3 <e LE Event

HCI Event

com3@115200

[3E 1E ]: 02 01 00 01 65 B3 2A 8B 68 49 12 02 01 1A 02 0A 0C 0B FF 4C 00 10 06 01 1A A2 F9 7F D5 A3

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "49688B2AB365"

Data_Len[0] = 0x12 (18)

Data[0] = "02 01 1A 02 0A 0C 0B FF 4C 00 10 06 01 1A A2 F9 7F D5"

RSSI[0] = 0xA3 (-93, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.299 com3 <e LE Event

HCI Event

com3@115200

[3E 1F ]: 02 01 00 01 27 3F E1 AF 7E 40 13 02 01 1A 02 0A 0C 0C FF 4C 00 10 07 17 1F 08 0E B7 CD 38 AF

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "407EAFE13F27"

Data_Len[0] = 0x13 (19)

Data[0] = "02 01 1A 02 0A 0C 0C FF 4C 00 10 07 17 1F 08 0E B7 CD 38"

RSSI[0] = 0xAF (-81, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.308 com3 <e LE Event

HCI Event

com3@115200

[3E 1D ]: 02 01 00 01 DB 71 9E 00 03 5D 11 02 01 1A 02 0A 18 0A FF 4C 00 10 05 06 18 7C 11 DB B0

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "5D03009E71DB"

Data_Len[0] = 0x11 (17)

Data[0] = "02 01 1A 02 0A 18 0A FF 4C 00 10 05 06 18 7C 11 DB"

RSSI[0] = 0xB0 (-80, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.326 com3 <e LE Event

HCI Event

com3@115200

[3E 1D ]: 02 01 00 01 B5 BE 5C 41 96 51 11 02 01 1A 02 0A 0C 0A FF 4C 00 10 05 41 1C 87 25 FA A2

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "5196415CBEB5"

Data_Len[0] = 0x11 (17)

Data[0] = "02 01 1A 02 0A 0C 0A FF 4C 00 10 05 41 1C 87 25 FA"

RSSI[0] = 0xA2 (-94, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.329 com3 <e LE Event

HCI Event

com3@115200

[3E 1A ]: 02 01 00 00 7D 96 B9 66 1B 00 0E 02 01 02 02 0A F4 07 03 0A 18 0F 18 CE FD A0

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x0 (0, "Public Address")

Address[0] = "001B66B9967D"

Data_Len[0] = 0xE (14)

Data[0] = "02 01 02 02 0A F4 07 03 0A 18 0F 18 CE FD"

RSSI[0] = 0xA0 (-96, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.364 com3 <e LE Event

HCI Event

com3@115200

[3E 21 ]: 02 01 00 00 DC BC A0 37 60 00 15 02 01 06 11 07 FB 34 9B 5F 80 00 00 80 02 10 00 00 E9 FE 00 07 A4

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x0 (0, "Public Address")

Address[0] = "006037A0BCDC"

Data_Len[0] = 0x15 (21)

Data[0] = "02 01 06 11 07 FB 34 9B 5F 80 00 00 80 02 10 00 00 E9 FE 00 07"

RSSI[0] = 0xA4 (-92, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.407 com3 <e LE Event

HCI Event

com3@115200

[3E 1D ]: 02 01 00 01 12 A1 AD E3 84 76 11 02 01 1A 02 0A 0C 0A FF 4C 00 10 05 51 1C A3 27 A7 B4

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "7684E3ADA112"

Data_Len[0] = 0x11 (17)

Data[0] = "02 01 1A 02 0A 0C 0A FF 4C 00 10 05 51 1C A3 27 A7"

RSSI[0] = 0xB4 (-76, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.421 com3 <e LE Event

HCI Event

com3@115200

[3E 1D ]: 02 01 00 01 B8 46 CF 35 3B 7B 11 02 01 1A 02 0A 0C 0A FF 4C 00 10 05 03 18 AD F2 CC B9

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "7B3B35CF46B8"

Data_Len[0] = 0x11 (17)

Data[0] = "02 01 1A 02 0A 0C 0A FF 4C 00 10 05 03 18 AD F2 CC"

RSSI[0] = 0xB9 (-71, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.423 com3 <e LE Event

HCI Event

com3@115200

[3E 1D ]: 02 01 00 01 B0 A4 F7 61 F2 67 11 02 01 1A 02 0A 06 0A FF 4C 00 10 05 73 1C 59 98 21 B7

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "67F261F7A4B0"

Data_Len[0] = 0x11 (17)

Data[0] = "02 01 1A 02 0A 06 0A FF 4C 00 10 05 73 1C 59 98 21"

RSSI[0] = 0xB7 (-73, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:27.687 com3 <e LE Event

HCI Event

com3@115200

[3E 21 ]: 02 01 00 00 19 43 AF 38 C1 A4 15 02 01 06 11 16 95 FE 30 58 5B 05 01 19 43 AF 38 C1 A4 28 01 00 BE

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x0 (0, "Public Address")

Address[0] = "A4C138AF4319"

Data_Len[0] = 0x15 (21)

Data[0] = "02 01 06 11 16 95 FE 30 58 5B 05 01 19 43 AF 38 C1 A4 28 01 00"

RSSI[0] = 0xBE (-66, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:28.012 com3 <e LE Event

HCI Event

com3@115200

[3E 2B ]: 02 01 00 01 B3 CA AD 5C 96 DB 1F 02 01 06 1B FF 57 01 00 13 AE 52 08 B9 8F B3 B5 20 BB 44 8A A0 F2 E0 24 01 DB 96 5C AD CA B3 AA

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "DB965CADCAB3"

Data_Len[0] = 0x1F (31)

Data[0] = "02 01 06 1B FF 57 01 00 13 AE 52 08 B9 8F B3 B5 20 BB 44 8A A0 F2 E0 24 01 DB 96 5C AD CA B3"

RSSI[0] = 0xAA (-86, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:28.102 com3 <e LE Event

HCI Event

com3@115200

[3E 20 ]: 02 01 00 00 8A 23 F2 DC 1B 00 14 02 01 02 03 02 00 18 0C 09 50 54 53 2D 53 4D 2D 38 41 32 33 C9

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x0 (0, "Public Address")

Address[0] = "001BDCF2238A"

Data_Len[0] = 0x14 (20)

Data[0] = "02 01 02 03 02 00 18 0C 09 50 54 53 2D 53 4D 2D 38 41 32 33"

RSSI[0] = 0xC9 (-55, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:28.603 com3 <e LE Event

HCI Event

com3@115200

[3E 1E ]: 02 01 00 01 B8 7F C9 7B D7 56 12 02 01 1A 02 0A 08 0B FF 4C 00 10 06 77 1D 43 01 40 38 A7

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "56D77BC97FB8"

Data_Len[0] = 0x12 (18)

Data[0] = "02 01 1A 02 0A 08 0B FF 4C 00 10 06 77 1D 43 01 40 38"

RSSI[0] = 0xA7 (-89, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:29.698 com3 <e LE Event

HCI Event

com3@115200

[3E 28 ]: 02 01 00 01 C4 70 1F D7 CD 44 1C 02 01 06 11 07 23 20 56 7C 05 CF 6E B4 C3 41 77 28 51 82 7E 1B 06 09 48 65 6C 6C 6F B7

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x1 (1, "Random Address")

Address[0] = "44CDD71F70C4"

Data_Len[0] = 0x1C (28)

Data[0] = "02 01 06 11 07 23 20 56 7C 05 CF 6E B4 C3 41 77 28 51 82 7E 1B 06 09 48 65 6C 6C 6F"

RSSI[0] = 0xB7 (-73, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:30.309 com3 <e LE Event

HCI Event

com3@115200

[3E 1F ]: 02 01 00 00 07 BF 01 38 C1 A4 13 02 01 06 0F 16 95 FE 30 58 5B 05 E2 07 BF 01 38 C1 A4 08 A8

event = 0x3E (62,"LE Event")

LE_Event_Code = 0x2 (2, "LE Advertising Report Event")

Num_Reports = 0x1 (1)

Event_Type[0] = 0x0 (0, "Connectable Undirected Event")

Address_Type[0] = 0x0 (0, "Public Address")

Address[0] = "A4C13801BF07"

Data_Len[0] = 0x13 (19)

Data[0] = "02 01 06 0F 16 95 FE 30 58 5B 05 E2 07 BF 01 38 C1 A4 08"

RSSI[0] = 0xA8 (-88, 127 means RSSI is not available, Range from -127 to 20 dbm)

 

 

09/16/21 08:52:31.740 com3@115200 c> LE_Set_Scan_Enable

HCI Command

com3@115200

[0C 20 02 ]: 00 01

opcode = 0x200C (8204, "LE_Set_Scan_Enable")

LE_Scan_Enable = 0x0 (0, "Scanning is disabled")

Filter_Duplicates = 0x1 (1, "Duplicate filtering is enabled")

 

 

09/16/21 08:52:31.746 com3 <c LE_Set_Scan_Enable

HCI Command Complete Event

com3@115200

[0E 04 ]: 01 0C 20 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x200C (8204, "LE_Set_Scan_Enable")

Status = 0x0 (0, "Success", "Success")

 

 

09/16/21 08:52:52.374 com3@115200 c> LE_Create_Connection

HCI Command

com3@115200

[0D 20 19 ]: 64 00 32 00 00 00 8A 23 F2 DC 1B 00 03 02 00 02 00 00 00 0A 00 00 00 00 00

opcode = 0x200D (8205, "LE_Create_Connection")

LE_Scan_Interval = 0x64 (100, in slots. Range: 2.5ms to 10.25s)

LE_Scan_Window = 0x32 (50, in slots. Range: 2.5ms to 10.25s)

InitiatorFilterPolicy = 0x0 (0, "White List not used and the Peer address in this command is used")

Peer_Address_Type = 0x0 (0, "Public Address")

Peer_Address = "001BDCF2238A"

Own_Address_Type = 0x3 (3, "RPA or Random Address")

Conn_Interval_Min = 0x02 (2)

Conn_Interval_Max = 0x02 (2)

Conn_Latency = 0x00 (0)

Supervision_Timeout = 0x0A (10)

Minimum_CE_Len = 0x00 (0, in slots. Range:1 to 2*Conn_Interval)

Maximum_CE_Len = 0x00 (0, in slots. Range:1 to 2*Conn_Interval)

 

 

09/16/21 08:52:52.382 com3 <e Command Status

HCI Event

com3@115200

[0F 04 ]: 0C 01 0D 20

event = 0x0F (15,"Command Status")

Status = 0xC (12, "Command Disallowed", "Command Disallowed")

 

 

0 Likes
DheerajPK_41
Moderator
Moderator

Hi,

As per the spec, the controller shall return "Command Disallowed (0x0C)" error code If the Host issues HCI_LE_Create_Connection command when another HCI_LE_Create_Connection command is pending in the Controller.  Please confirm it is not so in your testing.

I could also reproduce similar issue. We will check this with our firmware team. 

 

Could you please let us know the scenario where you uses Own_Address_Type = 0x3 (3, "RPA or Random Address")?

 

Thanks,

-Dheeraj.P.K

View solution in original post

0 Likes
tado_4837711
New Contributor II

Hi,

I am quiet sure "HCI_LE_Create_Connection command when another HCI_LE_Create_Connection command is pending in the Controller" is not our situation.

Our scenario is quiet simple, SM test cases:

SM/PER/KDU/BI-02-C [LE Legacy Pairing, IUT Responder – Key Rejected]
SM/CEN/KDU/BI-02-C [LE Legacy Pairing, IUT Initiator – Key Rejected]
SM/PER/KDU/BI-03-C [LE Secure Connections Pairing, IUT Responder – Key Rejected]
SM/CEN/KDU/BI-03-C [LE Secure Connections Pairing, IUT Initiator – Key Rejected]

requires IRK bit set which indicates that the The IUT distributes the IRK. Thus we need HCI_LE_Create_Connection with Own_Address_Type = 0x3.

We have also tested with another Controller, it works as expected:

tado_4837711_0-1632707477082.png

 

0 Likes
DheerajPK_41
Moderator
Moderator

Hi,

This issue is under debug now. Please expect some delay. 

Thanks,

-Dheeraj.P.K

0 Likes
DheerajPK_41
Moderator
Moderator

Our firmware team is debugging it. The fix will be available in the next SDK only.

0 Likes