- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I connected External Host MCU to CYBT-483056-02 module thru UART lines and like to transfer serial data using CYSPP mode.
XRES of CYBT-483056-02 set to High, CYSPP pin set to High for put into command mode.
When I Reset the module and monitor the UART_TX pin using an oscilloscope during the boot process. If the module boots normally, the system_boot (BOOT, ID=2/1) API event should occur but I couldn't see any response & event from UART_TX pin. When I send /RFAC command from Host MCU, I am not getting any response from CYBT-483056-02 module. Is there any settings / configurations on special function pins and CYBT-483056-02 module?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Could you please confirm whather you have done all the steps mentioned in the user guide or not? Detailed steps are given in the document.
To start CYSPP operation, I think we need to assert (LOW) the CYSPP pin. That's what I can see in the document. Please check it once.
Thanks,
-Dheeraj.P.K
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Could you please confirm whather you have done all the steps mentioned in the user guide or not? Detailed steps are given in the document.
To start CYSPP operation, I think we need to assert (LOW) the CYSPP pin. That's what I can see in the document. Please check it once.
Thanks,
-Dheeraj.P.K
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you for your response.
I believe I have followed the steps provided in the user guide document. UART TX,RX,CTS and RTS pins are connected to external Host MCU as given in the document.
EZ-Serial’s UART interface has two required signals for data and two optional signals for flow control, if enabled:
Required: RXD – Receive data (input), connect to host TXD (output)
Required: TXD – Transmit data (output), connect to host RXD (input)
Optional: RTS – Module-side flow control (output), connect to host CTS (input), default enabled
Optional: CTS – Host-side flow control (input), connect to host RTS (output), default enabled
Before enter into CYSPP mode, I would like to configure the CYBT-483056-02 module such as reset the module , setting of transmit power, device name etc so that I have set CYSPP pin to HIGH to put into Command mode.
CYSPP pin externally de-asserted (HIGH): Command mode (text or binary)
CYSPP pin externally asserted (LOW): CYSPP mode
Whenever I send any API command from Host MCU like /RFAC , GBA , I am not seeing any response from BLE module.
Is there a way to find out whether module is pre-programmed with EZ-Serial Firmware?
I am not sure whether I missed any settings on HW pins. Have we required to control CTS , RTS pins while transmit commands or receive response/event?
Thanks,
MuthuKumar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Muthu,
When EZ-Serial is programmed and module powered, you will be able to see the module advertising using CySmart app along with the xx:xx:xx address.
Scott