Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AIROC™ Bluetooth Forum Discussions

BeKi_4844661
Level 3
Level 3
25 sign-ins 10 replies posted 10 questions asked

Dear Cypress.

I did set-up for CYW720719-EVB through wiced studio.

then How can I listen to streaming media?

Is this have to HW change the EVB board?

Could you provide HW set-up manual for listen to streaming media?

thank you.

0 Likes
8 Replies
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi @BeKi_4844661 ,

You don't need to do any hardware changed on the CYW20719 eval board. You can refer to /20719-B1_Bluetooth/apps/demo/watch example in WICED Studio for audio implementation using CYW20719.

0 Likes

Dear Cypress.

Where can i connect Audio speaker for listening Audio in CYW720719-EVB  board?

And A2DP SNK role demo not found in Wiced studio.

Could you check it please?

0 Likes

As mentioned in WICED Bluetooth Software Features  , CYW20719 do not support A2DP sink functionality. Please use CYW20706 or CYW20721B2 solutions for audio applications.

0 Likes

I understand A2DP sink functionality.

Where can i connect Audio speaker for listening Audio in CYW720719-EVB board?

Could you Provide HW set-up method in Audio speaker Pin of CYW720719-EVB & CYW920706WCDEVAL Board?

0 Likes

If you are trying to connect a Bluetooth speaker to CYW207219 board, that means you are trying to configure it as A2DP sink right? So this feature is not available on CYW20719.

For CYW20706, please let me know the audio codec you are using. 

0 Likes

I used SBC codec in CYW920706WCDEVAL Board.

And I want to connect Speaker for listen to streaming media.

but How can connect Speaker in CYW920706WCDEVAL Board?

 

0 Likes

CYW20706 headset app cannot connect with speaker since Headset itself act as A2DP sink.

Also, SBC codec is a Bluetooth default codec, you will need an external codec in order to translate pcm/i2s input to audio output. 

 

 

0 Likes

 

 


Dear Cypress.

I want listen audio streaming to use SBC codec through  CYW920706WCDEVAL Board.

And I will be going to connect Audio amp in CYW920706WCDEVAL Board.

but How can I setting for CYW920706WCDEVAL Board?

Need HW jumper? else Need HW pin setting?

0 Likes